Skip to main content
Visitor II
Oct 22, 2026 5:24 AM UTC
Question

Unable to load STUSB4531 GUI firmware on NUCLEO-C071RB (insufficient drive space when copying .bin file)

Hello,

I am trying to configure an STUSB4531 using the STUSB4531 GUI and a NUCLEO-C071RB board as the I²C bridge.

Following the application note/documentation, I connected the NUCLEO board to my PC and attempted to drag and drop the provided firmware .bin file onto the board's mass-storage device. However, Windows reports that there is not enough free space available on the drive.

Details:

  • Board: NUCLEO-C071RB
  • Target Device: STUSB4531
  • Method: NUCLEO board used as I²C bridge for the STUSB4531 GUI
  • Firmware file size: ~43 KB
  • Available space on the NUCLEO mass-storage drive: only ~7-8 KB

When I inspect the drive exposed by the NUCLEO board, it appears almost full, leaving significantly less space than the firmware binary size. As a result, the drag-and-drop operation fails.

My questions are:

  1. Is the firmware supposed to be copied directly to the mass-storage drive, or should it be programmed using another method such as STM32CubeProgrammer?
  2. Is the limited reported drive capacity normal for the NUCLEO-C071RB?
  3. Do any existing files on the drive need to be removed first?
  4. Is there a specific firmware version or procedure required for using the NUCLEO-C071RB as an I²C bridge with the STUSB4531 GUI?

Has anyone successfully programmed the required bridge firmware onto a NUCLEO-C071RB and used it with the STUSB4531 GUI? If so, could you please share the correct flashing procedure?

Thank you for your help.

2 replies

Mike_ST
ST Technical Moderator
Oct 22, 2026 1:30 PM UTC

Hello,

>> 1 ) Is the firmware supposed to be copied directly to the mass-storage drive, or should it be programmed using another method such as STM32CubeProgrammer?
Both should work, try with STM32CubeProgrammer in case drag&drop fails for some reason.

>> 2) Is the limited reported drive capacity normal for the NUCLEO-C071RB?
Yes, it is not depending on the flash size of the MCU, you can have 1MB flash on the MCU, but, as example, Windows might report: "Used space: 24KB, Free Space : 8KB"
Reported drive size is meaningless in that context.

>> 3) Do any existing files on the drive need to be removed first?
No need to delete them,
you should always see 2 persisting files: DETAIL.TXT + GETSTART.HTM

>> 4) Is there a specific firmware version or procedure required for using the NUCLEO-C071RB as an I²C bridge with the STUSB4531 GUI?
I personally don't have answer for this one as I never used this boards. The one you have should work.

>> Has anyone successfully programmed the required bridge firmware onto a NUCLEO-C071RB and used it with the STUSB4531 GUI? If so, could you please share the correct flashing procedure?

As said above please try to STM32CubeProgrammer if drag&drop fails, 
STM32CubeProgrammer might require you to specify the flash start address of 0x08000000 when flashing a bin file.

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. 
Pavel A.
Oct 23, 2026 11:45 PM UTC

Please try copying the file from command line (cmd.exe copy command or powershell) rather than by drag & drop.

If the emulated flash drive indeed exposes less free space than the file size, it is undocumented behavior, with obvious consequences.