Skip to main content
Associate
May 14, 2026 6:35 AM UTC
Question

Unable to halt/connect STM32H7S3L8 using external debugger on Nucleo-H7S3L8 (JP1 closed)

Hi everyone,

I'm facing issues connecting an external debugger to the NUCLEO-H7S3L8 board (STM32H7S3L8).

Current Setup:

  • Board powered via CN5 (ST-LINK USB)
  • JP1 closed (to disable on-board ST-LINK)
  • External debugger connected to CN1 (MIPI20 connector)
  • SWD mode at low speed (500 kHz to 1 MHz)
  • Correct power sequence: Power CN5 first → wait for COM LED (LD8) to stabilize → then connect external probe

What I have already tried:

  • BOOT0 = 1 (jumper on CN11[5-7]) to enter bootloader mode and halt using external debugger
  • Internal ST-LINK works fine when JP1 is open (using STM32CubeProgrammer)

    Problem:

    The external debugger is unable to connect or halt the CPU, please guide me how to fix it.

    Thanks,
    regards,
    Surender.

2 replies

AScha.3
Super User
May 14, 2026 5:09 PM UTC

Hi,

what is your external debugger ?

>external debugger is unable to connect or halt the CPU

Which program + debug probe ?

If you feel a post has answered your question, please click on " Best Answer ".
surenderAuthor
Associate
May 21, 2026 3:54 PM UTC
Hi,
I solved my problem:
When I used APSEL=1 I was able to halt the CPU.
Debug probe was a 20-pin SWD debug probe.
External debugger was PALMICE.