Skip to main content
arnold_w
Senior II
July 14, 2025
Question

Unable to get USB_OTG_HS host on PB14/PB15 on Nucleo board to react

  • July 14, 2025
  • 3 replies
  • 418 views

I'm working with the NUCLEO -F 446ZE MB1137 B-01 development board. My goal is to make a Virtual Com Port tunnel, where I plug in PA11/PA12 (USB device) to a PC and PB14/PB15 (USB host) to another product my company makes. I want to use the full speed (12 MBits/s) on both USB peripherals. It was very straight-forward to get the USB device to work using STM32CubeIDE, but no matter what I do I can't get the USB host to work. To isolate the problem, I removed the USB device completely and I’m currently only focusing on the USB host. I've added some logging here and there (using a sw bit-bang UART) e.g. in USBH_UserProcess, USBH_CDC_ClassRequest, OTG_HS_IRQHandler and in case of errors in MX_USB_HOST_Init. I have set PG6 high (right after the call to MX_USB_HOST_Init) to enabled VBUS on the CN13 connector (and measured 5 V on the 4th pin on a micro-USB to USB-A-female connector) and LED LD8 shows green light and LED LD7 (over-current indicator) never lights up. I'm using HSE 8 MHz and I make sure to multiply and divide it properly so that USB gets 48 MHz in the clock tree. Still, it seems the firmware is not reacting at all when I plug something into connector CN13. I've tried plugging in my company’s product, an FTDI USB-to-serial cable, and an optical mouse (its LED on the bottom did not light up). Does anybody know what I'm doing wrong?

Connectivity USB_OTG_HS:
External Phy: Disable (grayed out)
Internal FS Phy: Host_Only
Activate_SOF: Unchecked
Activate_VBUS: Unchecked
Speed: Host Full Speed 12MBit/s
Enable internal IP DMA: Disabled
Physical interface: Internal Phy
Signal start of frame: Disabled
User constants: None
USB On The Go HS End Point 1 Out global interrupe: Unchecked
USB On The Go HS End Point 1 In global interrupt: Unchecked
USB On The Go HS global interrupt: Checked. Prio 5, subprio 0
PB14 USB_OTG_HS_DM n/a Alternate Function Push Pull No pull-up and no pull-down Very High
PB15 USB_OTG_HS_DP n/a Alternate Function Push Pull No pull-up and no pull-down Very High

USB_HOST:
Class For HS IP: Communication Host Class (Virtual Port Com)
Class For HS IP: Disable (Grayed out; I can’t select anything else)
USBH_MAX_NUM_ENDPOINTS (Maximum number of endpoints): 2
USBH_MAX_NUM_INTERFACES (Maximun number of interfaces): 2
USBH_MAX_NUM_SUPPORTED_CLASS (Maximun number of supported class): 1
USBH_MAX_NUM_CONFIGURATION (Maximun number of supported configuration): 1
USBH_KEEP_CFG_DESCRIPTOR (Keep the configuration into RAM): Enabled
USBH_MAX_SIZE_CONFIGURATION (Maximun size in bytes for the Configuration Descriptor): 256 bytes
USBH_MAX_DATA_BUFFER (Maximun size of temporary data): 512 bytes
USBH_DEBUG_LEVEL (USBH Debug Level): 0: No debug message
USBH_USE_OS (Enable the support of an RTOS): Enabled
USBH_PROCESS_PRIO (The CMSIS-RTOS osPriority value specifies the priority for the USB Host thread): priority: normal (default)
USBH_PROCESS_STACK_SIZE (The CMSIS-RTOS stack size requirements in words): 128
Drive_VBUS_HS GPIO Output PG6 [USB_PowerSwitchOn[STMPS2151STR_EN]]

This topic has been closed for replies.

3 replies

ST Technical Moderator
July 14, 2025

Hi @arnold_w 

Did you test the same controller USB_OTG_HS using PB14/PB15 in device mode? If working without issues, you may refer to this example in host mode.

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL
arnold_w
arnold_wAuthor
Senior II
July 15, 2025

So, it turns out CN13 wasn't connected to the PB14/PB15 USB peripheral, it was connected to the PA11/PA12 USB peripheral instead. Now I've abandoned the CN13 connector and I'm connecting directly to PB14/PB15. Configuring both USB peripherals as devices worked great, but when I configure the PB14/PB15 USB peripheral as a host and plug in a device, then I get a HardFault. This is surprising because I've made very few changes to the code Cube generated for me. Is there perhaps some define/configuration I have forgotten to set since I want to run with FreeRTOS? Here's the stack trace when it crashes:

HardFault_Handler() at stm32f4xx_it.c:88 0x80019f6
<signal handler called>() at 0xfffffff1
memcpy() at 0x80118e6
prvCopyDataToQueue() at queue.c:2,102 0x800e444
xQueueGenericSendFromISR() at queue.c:995 0x800e0d2
osMessageQueuePut() at cmsis_os2.c:1,766 0x800d888
USBH_LL_PortEnabled() at usbh_core.c:1,235 0x800c43e
HAL_HCD_PortEnabled_Callback() at usbh_conf.c:183 0x80111c4
HCD_Port_IRQHandler() at stm32f4xx_hal_hcd.c:1,687 0x800390e
HAL_HCD_IRQHandler() at stm32f4xx_hal_hcd.c:559 0x800271a

arnold_w
arnold_wAuthor
Senior II
July 15, 2025

It appears the default stack size (USBH_PROCESS_STACK_SIZE) was too small, I had to increase it from 128 to 512 to avoid the HardFault.