Skip to main content
Cpatt.1
Associate II
November 12, 2022
Question

Unable to connect and flash program to STM32F407(custom board)

  1)is crystal is required to be used for program flashing 

2) boot0 to be low or High

Note: I'm using ST-LINK V2

​

​

This topic has been closed for replies.

2 replies

Tesla DeLorean
Guru
November 12, 2022

It doesn't need an external crystal as it runs from HSI.

The BOOTx pin shouldn't make a lot of difference unless the user code sleeps the device or reconfigures pins.

​

M​ore likely you're not powering it properly, issues with VDDA or VCAP

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
MM..1
Super User
November 12, 2022

How stlink you use explain SWD connection show photo...