Skip to main content
JDirk.1
Associate III
Aug 18, 2020 5:01 PM UTC
Solved

UART using st-link v2-1 break up from Nucleo F446RE

Hello,

the UART is not working.

st-link is stand alone (not connected to Nucleo anymore)

i am using a separate stm32f446ret6, tx(PIN16) and rx (PIN17) are connected to CN3 (TX/RX).

in addition the SWD CN4 of the st-link is used (all connections are made to the uC).

Programming is working fine. COM port is shown once i connect the st-link but tera term is showing nothing.

going back to a second board where the st-link is still part of the Nucleo (not break up) everything is working, uart is working.

What do you need to know to support me?

This topic has been closed for replies.
JDirk.1
JDirk.1Best answer
Associate III
Aug 18, 2020 6:50 PM UTC

problem solved: i connected the tx comming from the uC to the rx of the st-link and the rx from the uC to the tx of the uC.

of course that makes sense ^^

thank you very much!!

4 replies

Uwe Bonnes
Chief
Aug 18, 2020 5:14 PM UTC

Where is the ground connection? And as a test, does shorting CN3 echo the characters you type in the terminal?

JDirk.1
JDirk.1Author
Associate III
Aug 18, 2020 6:34 PM UTC

ground is connected from CN4 (SWD) PIN 3 to ground of the uC (i think 5 times, at least 1 ground per side).

what do you mean by echo? how can i check that? i guess a multimeeter is not usable?

JDirk.1
JDirk.1Author
Associate III
Aug 18, 2020 6:40 PM UTC

if i connect Tx and Rx on CN3 (both lines together) nothing is happening on the terminal

JDirk.1
JDirk.1AuthorBest answer
Associate III
Aug 18, 2020 6:50 PM UTC

problem solved: i connected the tx comming from the uC to the rx of the st-link and the rx from the uC to the tx of the uC.

of course that makes sense ^^

thank you very much!!