Skip to main content
Associate II
March 14, 2025
Question

UART_HyperTerminal_IT Example on STM32N6570-DK Board - Debugger can't connect

I built and debugged the default example UART_HyperTerminal_IT using the STM32N6570-DK board, but the following error occurred. How can I resolve this issue? I am using the latest versions of ST-Link and all related software.

STMicroelectronics ST-LINK GDB server. Version 7.10.0

Copyright (c) 2025, STMicroelectronics. All rights reserved.

 

Starting server with the following options:

Persistent Mode : Disabled

Logging Level : 1

Listen Port Number : 61234

Status Refresh Delay : 15s

Verbose Mode : Disabled

SWD Debug : Enabled

 

Waiting for debugger connection...

Debugger connected

Waiting for debugger connection...

Debugger connected

Waiting for debugger connection...

This topic has been closed for replies.

4 replies

RomainR.
ST Employee
March 14, 2025

Hello @wwnsok2 

Do you changed STM32N6570-DK in DEV_BOOT mode to be able to debug it?
Check UM3300 section 7.7 Boot options
https://www.st.com/resource/en/user_manual/um3300-discovery-kit-with-stm32n657x0-mcu-stmicroelectronics.pdf

You can also you refer to this post:

https://community.st.com/t5/stm32-mcus-boards-and-hardware/nucleo-n657x0-q-failed-to-start-gdb-server/m-p/756600#M23206

Best regards,
Romain,

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
wwnsok2Author
Associate II
March 14, 2025
I set it to that mode, but it appears as shown in the attached photo.
RomainR.
ST Employee
March 14, 2025

@wwnsok2, the capture you shared doesn't help.

Can you confirm you configured BOOT0 and BOOT1 switch on STM32N6570-DK as the picture bellow:

RomainR_0-1741958865859.png

Then, press one time on NRST black button, LED2 Red must be ON and it confirms that STM32N6 is in DEV_BOOT mode. After that you can start a debug session.

Best regards,

Romain,

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
wwnsok2Author
Associate II
March 14, 2025
I proceeded with that mode, but I still get the same output result.