Skip to main content
MSaif
Associate
October 17, 2019
Question

Trace: No Synchronization in ST-Link Debugger Window for STM32F429I discovery board

Hi Everyone

I am trying to view variables in Keil MDK5 Logic Analyzer Window therefore I have enabled trace and do the required settings of my STM32F429I discovery board. But When I open Debug window and run my code I get trace: No Synchronization message at the bottom of MDK5 Debug window. Logic Analyzer window does not shoe any waveform of my variables. Please help me in fix this problem.

regards

hammi

This topic has been closed for replies.

2 replies

Tesla DeLorean
Guru
October 17, 2019

Make sure the SWO solder bridge is made on the back of the board.

Ensure that the trace frequency in the debug settings trace pane matches the speed you are running the core. Ie 168 MHz, or whatever.​

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
MSaif
MSaifAuthor
Associate
October 18, 2019

What SWO solder bridge Do I need to solder for SWO trace in STM32F429I Discovery board?