Skip to main content
DmtryVovk
Associate II
Mar 9, 2019 6:17 PM UTC
Solved

TIM2 remap causes an stlink error

Hello, please help me.

I use stm32f103rc mcu, stlink v2 and keil uvision5.

So executing

AFIO->MAPR |= AFIO_MAPR_TIM2_REMAP_FULLREMAP;

causes stlik connection error.

Algorithm:

  1. Flash the MCU with keil uvision.
  2. Step to remmaping line in code. In this stage everything works fine.
  3. "Cannot access target" "shutting down debug session"
  4. After this debugger no longer sees MCU. "No target connected" "error: target dll has been cancelled. Debugger aborted!"
  5. Connect to MCU under reset, erase flash.
This topic has been closed for replies.
Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Mar 9, 2019 7:36 PM UTC

One might guess that the TIM2 pins conflict with the JTAG or SWD pins PA13/PA14, etc.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..

4 replies

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Mar 9, 2019 7:36 PM UTC

One might guess that the TIM2 pins conflict with the JTAG or SWD pins PA13/PA14, etc.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
DmtryVovk
DmtryVovkAuthor
Associate II
Mar 9, 2019 7:42 PM UTC

Hi Clive, glad to meet you). No JTAG used, no SWD conflicted. 46SWDIO 49SWCLK 14,15,16,17 TIM2 remap to 50,55,29,30.

DmtryVovk
DmtryVovkAuthor
Associate II
Mar 10, 2019 7:37 AM UTC

Clive was wright. SWD turn off while execute

AFIO->MAPR |= AFIO_MAPR_TIM2_REMAP_FULLREMAP;

I use

__HAL_AFIO_REMAP_TIM2_ENABLE();

Instead. Is it because SWJ_CFG bits in AFIO_MAPR is only writable? How it worked in my old project?

Thank you.

Oladi
Associate II
Mar 18, 2019 3:58 PM UTC

I have a stm32f411re board and I have the same problem. But I don't know how to connect under reset mode and erase cpu, can u help me?

​

St-link utility or cube programmer erorr says "no stm32 found" or "cannot connect the target"

​

Also in the mass storage there is a fail document that says "the interface firmware failed to reset/halt the target mcu"