Skip to main content
Visitor
Nov 22, 2026 6:06 AM UTC
Question

The interface firmware FAILED to reset/halt the target MCU. (nucleo f446re)

I am using a NUCLEO-F446RE (MB1136 rev C) board with no external wires or shields connected, and I am consistently getting FAIL.TXT (The interface firmware FAILED to reset/halt the target MCU) on the NOD_F446RE drive, Target no device found (Reason: No device found on target) in STM32CubeIDE's ST-LINK GDB server, and Error: Unable to get core ID / Error: No STM32 target found! in STM32CubeProgrammer even though target voltage reads 3.24 V and STLink Virtual COM Port (COM5) and ST-Link Debug show up properly in Windows Device Manager. So far, I have verified the USB drivers, updated the on-board ST-LINK/V2-1 firmware to V2J46M33 (confirmed in DETAILS.TXT and STM32CubeProgrammer), checked the CN2 jumpers and U5V power jumper setting, inspected the back solder bridges, and tried connecting under reset / hardware reset at lower SWD frequencies, and I also noticed LD1 shifts from red to green after around 5 minutes of being powered, yet the target MCU still cannot be detected.

 


 

 

1 reply

MM..1
Super User
Nov 22, 2026 4:12 PM UTC

Dont use STLink Utility is oboslete… In programmer window before connect change mode from normal to Under reset.
And show yur booard connection …