Skip to main content
TLin.5
Associate III
Oct 18, 2025 12:37 PM UTC
Solved

T_VCC on STLinkV3 vs VCC on target

I have made an adapter that sits between the STLink V3 and the device that needs to be programmed, so that I can give T_VCC on the STLink side 3.3V from an external supply.

So far I have used 3.3V as VCC on the target as well, but I am considering lowering VCC on target to 3.0V instead.

As far as I can tell from datasheets, there shouldn't be an issue with keeping T_VCC on the STLink side at 3.3V while VCC on target is 3.0V, but I wanted to check here if anyone has something different to say about this mismatch.

 

If it's a bad idea, I will need to have adapters around with T_VCC 3.0V and others with T_VCC 3.3V depending on which target device I work with, which in this case is a bit of a hassle.

This topic has been closed for replies.
TDK
TDKBest answer
Oct 18, 2025 2:30 PM UTC

That will cause the ST-Link to send 3.3 V signals instead of 3.0 V, which is just on the threshold of okay, if internal pullups are used. If they are not used, there is even more margin.

TDK_0-1760797776089.png

So it'll be fine.

"If you feel a post has answered your question, please click ""Accept as Solution""."

2 replies

TDK
TDKBest answer
Oct 18, 2025 2:30 PM UTC

That will cause the ST-Link to send 3.3 V signals instead of 3.0 V, which is just on the threshold of okay, if internal pullups are used. If they are not used, there is even more margin.

TDK_0-1760797776089.png

So it'll be fine.

"If you feel a post has answered your question, please click ""Accept as Solution""."
TLin.5
TLin.5Author
Associate III
Oct 18, 2025 4:23 PM UTC

Thanks.

The programming pins are not used otherwise, so no internal pullups configured.