Skip to main content
Patrick Morwald
Associate III
February 5, 2018
Question

Switched my STM32F4 discovery and now Virtual Com port is not working

Posted on February 05, 2018 at 17:00

Hi,

i swapped my first STM32F407G-DISC1 discovery board for a new one and now the ST-Link onboard doesnt show up as a virtual com port in Windows 10 anymore. 

I flashed the St-Link with the new firmware, it runs V2.J30.S0 STM32 Debugger now.

I also installed the current Windows driver from 

http://www.st.com/content/st_com/en/products/development-tools/software-development-tools/stm32-software-development-tools/stm32-utilities/stsw-link009.html

.

Now i read the DISCOVERY boards dont all have the virtual com, but in

http://www.st.com/en/evaluation-tools/stm32f4discovery.html

it says that my order code should have it (on my PCB is a silk print next to the USB connector that says 'STM32F407G-DISC1).

Can it be that the silkscreen board code doesnt correspond to the 'order code' which is mentioned on the above website?

Please help since i really need the virtual COM port.

Patrick

#st-link-v2-1 #stm32f746-discovery #stm32f4
This topic has been closed for replies.

13 replies

Bogdan Golab
Lead
February 5, 2018
Posted on February 05, 2018 at 17:06

Run St-link utility to see firmware version. v2-1 is required (in this case v2-B

Bogdan Golab
Lead
February 5, 2018
Posted on February 05, 2018 at 17:13

The latest (DISC1) version shall have the st-link based on STM32F103CBT6 - the old  - STM32F103C8T6. Flash size matters  - bigger flash is needed for the ST-link/v2-B where the VCOM is implemented

Patrick Morwald
Associate III
February 12, 2018
Posted on February 12, 2018 at 10:19

Hi,

i have two boards, one of them doesnt instantiate the VCOM port, it has:

10:14:12 : ST-LINK SN : 066FFF535748775187133407

10:14:12 : ST-LINK Firmware version : V2J30S0

and the other board does instantiate it and has:

10:17:19 : ST-LINK SN : 066BFF3731324B4D43205239

10:17:19 : ST-LINK Firmware version : V2J25M14

Both boards are labeled MB997D / STM32F407G-DISC1 on the silkscreen and St-Link shows RevisionID: Rev 2.0 for both of them.

Can i upgrade the firmware of the non-working one to the firmware 

V2J25M14 or does it not fit the flash size?

Bogdan Golab
Lead
February 12, 2018
Posted on February 12, 2018 at 10:28

The standard way is to run  ST-LINK Utility and see after connecting to the target if the red message appears in the log - it will be stated if the upgrade is possible.

Just run the utility to see the checking results. Then you can upgrade the firmware from the same utility  - 'ST-LINK->Firmware Update' (sometimes you need to re-plug the USB cable when the tools complains about the connectivity).

If this does not help (I mean the ST-LINK Utility) more investigation will be required.

Tesla DeLorean
Guru
February 5, 2018
Posted on February 05, 2018 at 17:26

Are they different board revisions?

Pretty sure the MB997D instantiates the VCP, but it's not physically wired up to anything.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Bogdan Golab
Lead
February 5, 2018
Posted on February 05, 2018 at 17:37

Are you sure that MB997D applies to STMF429-DISC1?

Isn't it STM32F407G-DISC1 which has the MB997D?

Bogdan Golab
Lead
February 5, 2018
Posted on February 05, 2018 at 17:40

Sorry  - I have noticed that the boards is really F407