Skip to main content
Associate II
Aug 20, 2025 9:32 PM UTC
Question

STSW-LINK007 on FreeBSD

Hello world :)

Trying to upgrade firmware on series of STLINK-V3MODS on FreeBSD, downloaded 3.16.9 package from [1], after running:

java -jar STLinkUpgrade.jar

I got error message "Platform not supported (freebsd)".

Would it be possible to add support for FreeBSD? All should work as on Linux or macOS except serial port names here are /dev/cuaU0, /dev/cuaU1, etc. Ah I notices there are some dynamic libraries involved but these can be cross-compiled easily too let me know if you need support :)

Thanks :)

Tomek

[1] https://www.st.com/en/development-tools/stsw-link007.html

This topic has been closed for replies.

6 replies

Mike_ST
ST Technical Moderator
Aug 21, 2025 12:30 PM UTC

Hello,

As far as I know, there is no plan for the ST-Link upgrade tool to support FreeBSD.

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. 
CeDeROMAuthor
Associate II
Aug 21, 2025 12:41 PM UTC

Thanks @Mike_ST , how can I help to make this happen? Would it be possible to provide only firmware *.bin file so open-source tools can be used?

Mike_ST
ST Technical Moderator
Aug 21, 2025 1:34 PM UTC

Thank you for you help, but the STM32 ecosystem does not support FreeBSD, so I think it won't happen.

ST doesn't provide the binary file. You have to use the ST-Link Upgrade tool.

You can try to launch a linux VM under free BSD, maybe the upgrade process will work (never tried).

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.