Skip to main content
Explorer
February 21, 2024
Solved

STM32U585 VDDIO2

Hello Community,

I am using the STM32U585 in a design, and I have VDD at 3.3V and VDDIO2 at 1.8V.  The 1.8V rail is supplied by a 3.3V to 1.8V voltage regulator. I connected the Enable of this voltage regulator to one of the STM32U585 I/O (this I/O isn't on the PG port, because PG port is supplied by VDDIO2). Do you foresee any problem with this setup? I mean the 3.3V will turn on at first, and then the STM32 will turn on the 1.8V regulator, which supply VDDIO2 rail.  In the datasheet it is clear that, VDDIO2 and VDD are two independent supplies. I just want a confirmation, and if someone here has a similar implementation in a working design.

Thank you, Lamia

This topic has been closed for replies.
TDK
TDKBest answer
February 21, 2024

Confirmed, should work. Make sure you have a pulldown on the enable pin so it has a defined state when chip is in reset. VDDIO2 must be enabled in code as well.

"If you feel a post has answered your question, please click ""Accept as Solution""."

1 reply

TDK
TDKBest answer
February 21, 2024

Confirmed, should work. Make sure you have a pulldown on the enable pin so it has a defined state when chip is in reset. VDDIO2 must be enabled in code as well.

"If you feel a post has answered your question, please click ""Accept as Solution""."