Skip to main content
Associate II
August 11, 2025
Question

STM32N6570-DK Camera Issue

I've just received a brand new DK from Mouser and I've been trying to get the stock AI demo up and running. The camrea is connected, power is provided via a short USB-C cable on the 2nd USB connector (not the ST-Link one) and the jumpers changed over.

When I launch the AI demo via the touchscreen, the camera feed appears but there appears to be noise on the display. The camera stream appears for a few seconds before the screen greys out.

Video attached.

13 replies

Explorer
August 11, 2025

I have very similar issue. The only thing, I barely can see the camera feed, it disappears almost instantly after opening the demo.

Bought my kit directly from ST last week.

Tried powering with external USB-C adaptor and also through the DC bench supply using Arduino headers -> same result.

Also I have tried to re-flash out-of-the-box demo binary -> same result.

kevlarAuthor
Associate II
August 11, 2025

Ah, that's good that someone else is seeing a similar issue. 

Be interested to know whether this is a hardware/power issue on a certain batch of these boards.

Can anyone from ST comment, please?

kevlarAuthor
Associate II
August 12, 2025

@stmicro is anyone able to help with this please?

I'd appreciate the help as I'd like to start to use the DK as soon as possible

jiangfan
ST Employee
August 13, 2025

Hello, STM32N6570-DK the board itself should be OK, the issue should be mainly due to the AI demo software. Hopefully the issue may be resolved soon.

Visitor II
September 4, 2025

Hello,

i had a similar pb (STM32n6570-DK with MB1854B camera from Elektor STM32 Ai contest), and the boad crached when trying to use camera.

The demo was OK without the camera : message of camera missing OK.

I watched explanations from "Getting started with ST BrightSense on STM32N6" (https://www.youtube.com/watch?v=mWh26gPjXeg). So i was thinking about a software bug or camera cable (i have not exactly the same).

i reflashed a demo as explained : same pb.

So about the bord supply, i was always using the USB port from PC..... and you insit about power supply.

==> i tryed with an external usb supply, and the camera waked-uo ! Camera is running now !!!

Thanks for this discution ! 

Rmk : surprised that the camera use "many" current, in my mind the screen is more "gourmand" !

jiangfan
ST Employee
September 8, 2025

some explanations:

- when STM32n6570-DK is powered from STLINK USB port and PC via USB-A_to_USB-C cable, STLINK will limit current at 550mA

- STM32n6570-DK itself will consume about 400mA current, so adding MB1854B camera will consume more and over 550mA, hence it seems that the camera use "many" current

- user may USB-C_to_USB-C cable to power STM32n6570-DK, and STLINK will limit current at 1.66A or 3.2A depending on PC status, with this configuration no problem for STM32n6570-DK with MB1854B camera to work. 550mA/1.66A/3.2A of STLINK current limit is mentioned in STM32n6570-DK Schematics.

- user may also power STM32n6570-DK from STLINK USB port via USB-A_to_USB-C cable to USB charger, with this configuration no problem for STM32n6570-DK with MB1854B camera to work

Thierry GUILHOT
ST Employee
November 17, 2025

Hi All,

 

We have identified a screen display issue occurring when running the AI demo on certain products. The affected products belong to batches with batch numbers up to Z5C22001. In this batch code, the digit before the "C" represents the last digit of the year (for example, "5" corresponds to 2025), and the two digits following the "C" indicate the week number of that year (for example, "22" means week 22). Therefore, all batches with numbers earlier than week 22 of 2025 are impacted.

This issue is related to the memory driver and has been resolved in demo firmware version 1.3.0 and later. You can download the latest demo firmware from STM32CubeN6.

Best Regards,

Thierry,