Skip to main content
Adams.Peter
Associate III
Sep 26, 2017 8:21 PM UTC
Solved

STM32L496G-Discovery Unknown Device

Posted on September 26, 2017 at 22:21

My STM32L496G-Discovery shows up as an 'Unknown Device' in the Windows 7 Device manager.

I tried connecting to it with the ST-LINK Utility, it gives a 'No ST_LINK detected' error message.

Is there a way to directly connect to U6 (the 32F103 running ST-LINK firmware) over USB to do DFU?

#st-link #st-link-error
This topic has been closed for replies.
Vangelis Fortounas
Associate II
Sep 27, 2017 12:59 AM UTC
Posted on September 27, 2017 at 00:59

Is there a utility that will flash the encrypted ST-LINK FW through the SWD pins?

No there isn't exist such utility.

But, why are you convinced that chip is erased? It is very unusual.

Try to make a test

Plug your board to a computer

open device manager

right click to the unknown device(if exists such unknown device)

select properties

open Details tab

select from dropdown list the 'hardware id' 

observe for something like  USB\VID_0483&PID_374........  

If exists it's a matter of not installed drivers.

14 replies

Vangelis Fortounas
Associate II
Sep 26, 2017 8:41 PM UTC
Posted on September 26, 2017 at 22:41

Hello!

Try to install drivers from

http://www.st.com/content/st_com/en/products/development-tools/software-development-tools/stm32-software-development-tools/stm32-utilities/stsw-link009.html

.

There are several posts in this community about Installing drivers.

Is there a way to directly connect to U6 (the 32F103 running ST-LINK firmware) over USB to do DFU?

You mean that the STlink firmware is erased?

Regards

vf

Adams.Peter
Associate III
Sep 26, 2017 10:59 PM UTC
Posted on September 26, 2017 at 22:59

Yes, the drivers were installed, the '32F103 is not recognized as an ST-LINK device. 

Tesla DeLorean
Guru
Sep 26, 2017 11:30 PM UTC
Posted on September 26, 2017 at 23:30

Tried another cable, port, or system? What follows?

Pseudo CD/DVD Drive? DELL System? Intel filter driver?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
AMera
Associate
Jan 7, 2019 7:53 AM UTC

same problem

on a Gentoo Linux machine

Yesterday the atollicTrueStudio told me that the STLink firmeware on my STM32F411 Nucleo is old and there is an update available

-> OK

then i debugged a part of software ...all works for about 2houres

OK then i disconnected the board,

powered off my PC and today it doesn't work any more

the Program on the Target is still running like charm

BUT

there is no more connection

dmesg
 
 
[551559.359615] usb 11-4: USB disconnect, device number 6
 
[551563.688058] usb 11-4: new full-speed USB device number 7 using ohci-pci
 
[551563.967202] usb 11-4: New USB device found, idVendor=0483, idProduct=374b
 
[551563.967210] usb 11-4: New USB device strings: Mfr=1, Product=2, SerialNumber=3
 
[551563.967214] usb 11-4: Product: STM32 STLink
 
[551563.967217] usb 11-4: Manufacturer: STMicroelectronics
 
[551563.967220] usb 11-4: SerialNumber: 066AFF494851877267065831
 
[551563.969199] usb 11-4: can't set config #1, error -62
 
 
 

dmesg

[551559.359615] usb 11-4: USB disconnect, device number 6

[551563.688058] usb 11-4: new full-speed USB device number 7 using ohci-pci

[551563.967202] usb 11-4: New USB device found, idVendor=0483, idProduct=374b

[551563.967210] usb 11-4: New USB device strings: Mfr=1, Product=2, SerialNumber=3

[551563.967214] usb 11-4: Product: STM32 STLink

[551563.967217] usb 11-4: Manufacturer: STMicroelectronics

[551563.967220] usb 11-4: SerialNumber: 066AFF494851877267065831

[551563.969199] usb 11-4: can't set config #1, error -62

st-info --probe

setting new configuration (0 -> 1)

Found 1 stlink programmers

serial:

openocd: ""

flash: 0 (pagesize: 0)

sram: 0

chipid: 0x0000

descr: unknown device

so it looks like Atollic has, with this update, killed the STLink on my nucleo device :oops: :evil:

perhaps somebody knows how to fix this problem

AMera
Associate
Jan 7, 2019 8:02 AM UTC

NO DRIVER PROBLEM

another STM32F411 nucleo from the same batch

i bought 4 of this at the same time 3 working like charm

[583125.632133] usb 11-4: new full-speed USB device number 13 using ohci-pci

[583125.931172] usb 11-4: New USB device found, idVendor=0483, idProduct=374b

[583125.931175] usb 11-4: New USB device strings: Mfr=1, Product=2, SerialNumber=3

[583125.931176] usb 11-4: Product: STM32 STLink

[583125.931177] usb 11-4: Manufacturer: STMicroelectronics

[583125.931178] usb 11-4: SerialNumber: 066EFF494851877267013639

[583125.941190] usb-storage 11-4:1.1: USB Mass Storage device detected

[583125.941383] scsi host8: usb-storage 11-4:1.1

[583125.943287] cdc_acm 11-4:1.2: ttyACM0: USB ACM device

[583127.019180] scsi 8:0:0:0: Direct-Access    MBED    microcontroller 1.0 PQ: 0 ANSI: 2

[583127.019398] sd 8:0:0:0: Attached scsi generic sg5 type 0

[583127.029117] sd 8:0:0:0: [sde] 1056 512-byte logical blocks: (541 kB/528 KiB)

[583127.035123] sd 8:0:0:0: [sde] Write Protect is off

[583127.035126] sd 8:0:0:0: [sde] Mode Sense: 03 00 00 00

[583127.041129] sd 8:0:0:0: [sde] No Caching mode page found

[583127.041132] sd 8:0:0:0: [sde] Assuming drive cache: write through

[583127.121279] sd 8:0:0:0: [sde] Attached SCSI removable disk

JMora.7
Associate
Apr 18, 2022 1:56 PM UTC

Hi, I’m in the same situation here, brand new Nucleo board, and I get the following with

st-info — probe 
setting new configuration (0 -> 1)
Found 1 st-link programmers 
seria: XXXXXXXXXXXXXXXXXX < Edit 
flash: 0 (pagesize: 0)
sram: 0
chipid: 0x0000
descr: unknown device

It will not connect to the board.

Any procedure to resolve this?

Thanks,