Skip to main content
iHamd.1
Associate II
July 11, 2022
Question

STM32L452RET6 Question

Hi all,

I am using the STM32L452RET6 On my board and i have 2 quiestion regarding it:

1) VDD12 Net - how to set my hardware when i am not using external DC/DC? floating? GND? just a cap? if so what size?

2) when entering boot mode and going over the i/o voltage i noticed a few anomalies -

a) some USART legs were 3.3V and some not (USART1 both 0V, USART2 only one is 3.3V and USART3 Both were 3.3V) - why is that?

b) PA0 GPIO is 3.3V for some reason - why is that? couldn't find a purpose on datasheet.

Thanks in advance,

Ido

This topic has been closed for replies.

6 replies

waclawek.jan
Super User
July 11, 2022

Note, that there are two different versions of STM32L452RET6 - VDD12 pin is present only on models with external SMPS, i.e. with P suffix.

Pins in bootloader may have enabled internal pullups/pulldowns, see AN2606.

JW

iHamd.1
iHamd.1Author
Associate II
July 11, 2022

its the STM32L452RET6P vresion.

If External SMPS is not required, What do i do with it?

Amel NASRI
ST Technical Moderator
July 15, 2022

Hi @iHamd.1​ ,

I suggest you refer to the following application notes:

  • AN4555: Getting started with STM32L4 Series and STM32L4+ Series hardware development
  • AN4978: Design recommendations for STM32L4xxxx with external SMPS, for ultra-low-power applications with high performance

-Amel

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.
M4R10
Associate III
September 15, 2022

Hello,

here I have the same question about VDD12, leave floating or connect a cap to GND?

Can somebody says what we should do with this?

thanks

Piranha
Principal III
September 15, 2022

From AN4555.

Section 2.1 Power supplies:

VDD12 ... It does not need any external capacitance and cannot drive an external load.

Section 2.2 Power supply schemes:

As these VDD12 pin are also connected to internal regulators, they cannot accommodate a decoupling capacitance, neither can they be shared with an external circuitry for other purposes.

Figure 3. Power supply scheme: no components connected to VDD12.