Skip to main content
lukas239955_stm1_stmicro_com
Associate II
July 25, 2013
Question

STM32L151 flash size

Posted on July 25, 2013 at 16:17

Hi all,

I am using STM32L151CBU6 and STM32L151C8U6 with 128KB and 64KB Flash, respectively.

However, Atollic Truestudio (via ST-Link) is able to flash 88KB to the one with 64KB Flash and it seams working correctly. My own bootloader also flashes 88KB and it works.

It seems that C8U6 is just a ''renamed'' CBU6.

The only thing is that ST-Link utility sees C8U6 as 64KB target and does not allow to flash it over 64KB, but it reads full 128KB.

Does anyone have some experience about this?

Is it just the batch of C8U6 I have in hand?

Would it reliable enough? I guess ST can't guarantee it.

#st-link #flash-size
This topic has been closed for replies.

1 reply

emalund
Associate III
July 25, 2013
Posted on July 25, 2013 at 16:28

However, Atollic Truestudio (via ST-Link) is able to flash 88KB to the one with 64KB Flash and it seams working correctly.

 

the key word is 'seems'

 

 

It seems that C8U6 is just a ''renamed'' CBU6.Does anyone have some experience about this?

 

this is quite common, the 'trap' is that it may be a batch of 128k chips that exhibit a failure at some location above 64k but otherwise are OK

Would it reliable enough? I guess ST can't guarantee it.

 

see above

Erik