Skip to main content
Associate III
Jul 24, 2025 12:13 PM UTC
Solved

STM32H7S78-DK – Factory Application and BSP Example Issue

 

Dear ST Support,

I have two questions regarding the STM32H7S78-DK board.

1. Is it possible to retrieve the original factory application that comes preloaded on the STM32H7S78-DK? I’ve already flashed my own project, but as expected, this process erased the factory-provided firmware.

2. I tried programming the board using a BSP example selected via STM32CubeIDE’s Example Selector. However, the IDE fails to upload the example to the board. A pop-up briefly appears and then disappears, with no further feedback. Even when the board is disconnected, STM32CubeIDE doesn’t display any error or warning that the board is not connected.

Interestingly, when I run my own project, everything works as expected. The board is correctly flashed, and when it’s disconnected, I do receive the expected “ST-LINK not detected” message.

Best regards


 

 

KDJEM.1
KDJEM.1Best answer
ST Technical Moderator
Aug 18, 2025 10:39 AM UTC

Hello @Jorge Alves ,

 

Could you please try the following workaround to unblock the situation and let me know if the issue is solved or not:

- In the .project, delete the Appli nature from the natures block: <nature>com.st.stm32cube.ide.mcu.MCUAppliProjectNature</nature>

- Clean and rebuild the application

- Start a debug session

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.

10 replies

KDJEM.1
ST Technical Moderator
Jul 28, 2025 9:50 AM UTC

Hello @Jorge Alves ;

 

You can find the STM32H7S78-DKdemo in this link: STM32H7S78-DK - Discovery kit with STM32H7S7L8 MCU - STMicroelectronics. Please look at this post. 

To open BSP example, could you please use the latest STM32CubeIDE toolchain and follow these steps:

1- Click on File>open projects from File System

KDJEM1_0-1753695506980.png

 

2- Click on Directory 

KDJEM1_1-1753695506981.png

 

3. Choose the path of BSP example then click on Select Folder 

KDJEM1_5-1753696185309.png

4- Click on Finish

KDJEM1_4-1753696035108.png

 

I hope this help you.

Thank you.

Kaouthar

 

 

 

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.
Associate III
Jul 30, 2025 11:53 AM UTC

Hello, 

I followed these steps, but the problem persists. I tried running the example at version 1.18, and the BSP example worked, and programming the board was okay.

I think it can be a bug in your new version 1.19.

Best regards,
Jorge

KDJEM.1
ST Technical Moderator
Jul 31, 2025 8:03 AM UTC

Hello @Jorge Alves ;

 

I can reproduce the issue on my side and I reported internally for checking.

But, after click on "Clean Project" the issue is solved.

Could you please try to clean the project and let me know if the issue is solved or not?

KDJEM1_0-1753948733852.png

Internal ticket number: 215075 (This is an internal tracking number and is not accessible or usable by customers).

Thanks and best regards,

Kaouthar

 

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.
Associate III
Aug 13, 2025 5:26 PM UTC

I cleaned the project, but the issue is not solved.

KDJEM.1
ST Technical Moderator
Aug 14, 2025 7:46 AM UTC

Hello @Jorge Alves ,

 

I confirm the STM32CubeIDE1.19.0 issue.

This issue is currently being investigated by the STM32CubeIDE team.

 

Thank you.

Kaouthar  

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.
KDJEM.1
KDJEM.1Best answer
ST Technical Moderator
Aug 18, 2025 10:39 AM UTC

Hello @Jorge Alves ,

 

Could you please try the following workaround to unblock the situation and let me know if the issue is solved or not:

- In the .project, delete the Appli nature from the natures block: <nature>com.st.stm32cube.ide.mcu.MCUAppliProjectNature</nature>

- Clean and rebuild the application

- Start a debug session

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.
Associate III
Aug 26, 2025 3:42 PM UTC

Hello @KDJEM.1 

I tried that, and it worked. I also did this procedure in another project and solved the problem.


Thanks for the support.

KDJEM.1
ST Technical Moderator
Nov 28, 2025 10:19 AM UTC

Hello @Jorge Alves ;

 

The issue is fixed in STM32CubeIDE 2.0.0 version.

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.
KDJEM.1
ST Technical Moderator
Aug 27, 2025 7:29 AM UTC

Hello @Jorge Alves,

 

Glad to know that the issue is solved.

Are there other projects examples that have the same problem? Can you give the names of those projects?

 

Thank you for your contribution in STCommunity.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.
Associate III
Sep 5, 2025 6:06 AM UTC

@Jorge Alves  i am working with the STM32H7S78-DK board and I want to toggle the LEDs LD1 (PO1),However, when I try to flash my program into the development board, I get Failed to execute MI Command error, How can I flash my code to external flash memory? I will send you the LED [PO1] toggle code. Can you check the IOC? or else can you help me?