Skip to main content
Andreas Bolsch
Lead III
October 4, 2020
Question

STM32H7B3I-DK: Firmware for ISM43340-M4G-L44-10CF

UM2569 says:

"In STM32H7B3I-DK boards labeled A1945xxxx, the ISM43340-M4G-L44-10CF is loaded with the C3.5.2.6.STM.BETA4 version which allows a network scan only once. A new version of the ISM43340-M4G-L44-10CF firmware named C3.5.2.6.STM that fixes this limitation is available on the www.st.com website."

The present module indeed bears A1945..., however, a firmware dump shows

Product ID:  ISM43341-M4G-L44-SPI,  Firmware:  C3.5.2.6.STM, API:  v3.5.2.

Hence, it doesn't seem to be the BETA4 version??? Furthermore, on ST's website there is apparently no firmware. The only one I could find is

https://www.inventeksys.com/iwin/wp-content/uploads/ISM43340_M4G_L44_SPI_C3.5.2.6_DISCOVERY.zip

 Does the A1945... refer to board MB1486 or MB1332?

This topic has been closed for replies.