Skip to main content
Associate III
Jun 6, 2024 6:50 AM UTC
Solved

STM32H755 emmc compatibility - IS22TF08G-JCLA2

Hello,

In the RM0399 58.1 it is mentioned that EMMC is supported up to Version 4.51. I want to use the part  IS22TF08G-JCLA2 which supports a number of emmc interfaces up to 5.1 are these parts compatible? 

This topic has been closed for replies.
KDJEM.1
KDJEM.1Best answer
ST Technical Moderator
Jun 11, 2024 10:58 AM UTC

Hello @sarun ,

The HS200 mode supported in IS22TF08G is compatible with STM32H755.

KDJEM1_1-1718103452213.png

 

KDJEM1_0-1718103370314.png

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.

2 replies

KDJEM.1
KDJEM.1Best answer
ST Technical Moderator
Jun 11, 2024 10:58 AM UTC

Hello @sarun ,

The HS200 mode supported in IS22TF08G is compatible with STM32H755.

KDJEM1_1-1718103452213.png

 

KDJEM1_0-1718103370314.png

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.
sarunAuthor
Associate III
Jun 11, 2024 11:00 AM UTC

Thank you @KDJEM.1  for confirmation