Skip to main content
Associate
Apr 13, 2026 7:30 PM UTC
Solved

STM32H745I-DISCO touch screen stopped working after debugger crash

My STM32H745I-DISCO touch screen stopped working after a HardFault/debugger crash while running a test app generated by STM32CubeMX ("Create project from board"). The display works perfectly but touch is completely unresponsive.

Steps already taken:

  • Full chip erase + reflashed official FULL.hex (with MT25TL01G external loader)
  • Verified option bytes (RDP=AA, BCM4 and BCM7 both enabled)
  • Fixed reset mode from "Hardware reset" to "Software reset"
  • ST-LINK firmware is up to date (V3J17M10)
  • I2C4 registers show uninitialized on both cores

Display works, buttons visible, but no touch response at all.

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Apr 15, 2026 9:51 AM UTC

The issue is not quiet clear but since you are facing a Hardfault, the program is stopped, the screen displays something but all is frozen that's why you have the impression the touchscreen is unresponsive.

Read How to debug a HardFault on an Arm® Cortex®-M STM32

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

5 replies

mƎALLEm
ST Technical Moderator
Apr 15, 2026 8:44 AM UTC

Hello,


@lmmv_ml wrote:

My STM32H745I-DISCO touch screen stopped working after a HardFault/debugger crash


What does that mean? do you suspect the Hardfault broke the touchscreen module?

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
lmmv_mlAuthor
Associate
Apr 15, 2026 9:26 AM UTC

I am too new to this (embedded with STM32) to make any such assumption.

I just know:
* all was working on the board when I got it (demo, touch screen and all 3 samples apps

* ran a generated code app (generated by STM32CodeMX) in a Visual Studio Code STM32 setup which did not seem to work properly

* stopped the generated code app

* noticed issues with board (leds staying on when board stopped, etc)

* flashed the demo software back on the board

* screen does show the 3 samples apps

* touch screen not working (I do not have a mouse (with the right connector) that I can connect to validate if it does work with a mouse - as was suggested by some AI).

 

STM32CodeMX version: 6.17

board: STM32H745I-disco


Thank you for any help

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Apr 15, 2026 9:51 AM UTC

The issue is not quiet clear but since you are facing a Hardfault, the program is stopped, the screen displays something but all is frozen that's why you have the impression the touchscreen is unresponsive.

Read How to debug a HardFault on an Arm® Cortex®-M STM32

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
lmmv_mlAuthor
Associate
Apr 15, 2026 9:28 AM UTC

in my previous:
"...* noticed issues with board (leds staying on when board stopped, etc)..."

should read:

"...* noticed issues with board (leds staying on when the generated app stopped, etc)..."

lmmv_mlAuthor
Associate
Apr 15, 2026 11:10 AM UTC

Thank you, looking at that.