Question
STM32H745I-DISCO Board- I'm using IAR Workbench v 8.40.1 and the ST-LINK V3 shared mode does not work. I assume you need this mode to do dual-core debugging.
Has anyone been successful in enabling and using dual-core debugging of this H745I-DISCO board using the on-board ST-LINK v3 interface? I am able to use the interface to dowwnload and debug each core separately; however, I can't get the ST-LINK shared mode of dual-core debugging working with the so-called master and slave IAR workbench guis running concurrently.