Skip to main content
DGany.2
Associate
January 3, 2023
Question

STM32H743ZI2 NUCLEO board Ethernet doesn't work when moving to JP5 to 1.8V (MCU_VDD)

Hi All,

I use the STM32H743ZI2-NUCLEO board with JP5 on 1.8V for MCU_VDD.

Running the LWIP example, the Ethernet doesn't work (It does work when running with 3.3V).

Any idea how to make it work with 1.8V?

Thanks,

David

This topic has been closed for replies.

2 replies

KDJEM.1
ST Technical Moderator
January 12, 2023

Hello @Community member​,

Please make sure that  R4, R43, R44, R45, R46, R47, R48, R49, R50, R51, R52, R53, R59, R61, U1, U10, U15, and SB45 are not removed.

Because after removing these components, it becomes impossible to use Ethernet with1.8 V.

For more explanation, I advise you to refer at the UM2407.

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.
DGany.2
DGany.2Author
Associate
January 12, 2023

Hi Kaouthar,

Thanks for your reply.

The board is at its manufacturing state, no component was removed.

I just moved JP5 to 1.8V and the ETHERNET stopped working.

Any idea why?

Thanks,

David