Skip to main content
Associate
June 2, 2025
Question

STM32H735G-DK - No data from on-board MEMS PDM microphone (SAI4_A in Master Receive mode)

Hello,

I'm working on a project using the STM32H735G-DK development board. I'm trying to receive audio data from the on-board digital MEMS PDM microphone (U33) using SAI4 Block A in Master Receive mode. I selected PDM mode in CubeMX and configured SAI4_A as Master Receive. SAI4_CK2 is set as the clock output pin, and SAI4_D1 as the data input. I’m using PLL3P as the clock source for SAI4A, set to 49,152. Middleware PDM2PCM is enabled. I’m currently using HAL_SAI_Receive() (not DMA yet), but BDMA is enabled.

When I run the program, the microphone always returns a constant value (like 0xFF), or no data at all.

Has anyone successfully used the on-board PDM microphone with SAI4 on this board? What is required to activate the SAI4_CK2 clock and receive valid data?

 

Thanks for the help.

 

This topic has been closed for replies.

2 replies

Senior III
June 2, 2025

The onboard MP34DT05 is powered via VDD_MIC and enabled via MIC_CK, which is internally connected to SAI4_CK2.

If the clock is not toggling, the microphone stays inactive and outputs nothing or 0xFF.

EllaGezAuthor
Associate
June 3, 2025

In my code the clock is enabled, still wont work. The MIC gets 3.3V.