Question
STM32H573VIT3Q - Vcap pins have no voltage
- October 10, 2024
- 5 replies
- 2454 views
Hello Everyone :)
I have designed a custom board using STM32H573VIT3Q MCU. when I connected it with st link, the st link didn't recognize it.
After I checked the voltages on the power pins, I saw all the power pins were normal except the VCAP pin (not outputing voltage at all..about 50mV).
The Vcap capacitors P.N is (Digikey) : 490-GRM155Z71A225KE01DCT-ND
Attached schematic for more information.
Please your help.
(Note, FB1506 is a mistake, and is not assembled).
Thanks alot !