Skip to main content
alan239955_st
Associate II
Oct 12, 2024 6:51 PM UTC
Solved

STM32H573I DK STMod+ connector pin 18

The STM32H573I Discovery circuit diagram (MB1677) shows pin18 of the STMod+ connector going to PB12.

This should be the BOOT pin of the MXCHIP EMW3080B (MB1400)

But H5 Cube configures PB0 as BOOT

STM32Cube_FW_H5_V1.3.0\Projects\STM32H573I-DK\Applications\NetXDuo\Nx_Iperf_wifi\Core\Inc\main.h

#define MXCHIP_BOOT_Pin GPIO_PIN_0
#define MXCHIP_BOOT_GPIO_Port GPIOB

Is there a documentation error or have I got something wrong?

Thanks

 

This topic has been closed for replies.
STTwo-32
STTwo-32Best answer
ST Technical Moderator
Oct 14, 2024 5:32 PM UTC

Hello @alan239955_st 

Thank you so much for reporting. I can confirm it is a typo on the main.h file of the project. I've escalated to the concerned team for correction on the coming releases of the STM32CubeH5 (under internal ticket number 193702).

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

2 replies

STTwo-32
STTwo-32Best answer
ST Technical Moderator
Oct 14, 2024 5:32 PM UTC

Hello @alan239955_st 

Thank you so much for reporting. I can confirm it is a typo on the main.h file of the project. I've escalated to the concerned team for correction on the coming releases of the STM32CubeH5 (under internal ticket number 193702).

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
alan239955_st
Associate II
Oct 14, 2024 7:45 PM UTC

Thank you for the check @STTwo-32