Skip to main content
Associate II
Jan 23, 2024 8:11 AM UTC
Solved

STM32H573 & RS232

Hello Everyone, I am using STM32H573. Do we need to connect RS232 to UART transceiver or can we directly interface Rs232 signals with UART?

This topic has been closed for replies.
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Jan 23, 2024 8:27 AM UTC

Hello @madhu1 ,

Indeed you need a transceiver. Example: ST3232

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

4 replies

AScha.3
Super User
Jan 23, 2024 8:21 AM UTC

Hi,

CPU is at 0/+3,3V signal level, real RS232 maybe +/- 9 V signal ;

you need some interface, UART transceiver or similar. (without you damage the cpu ! )

If you feel a post has answered your question, please click on " Best Answer ".
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Jan 23, 2024 8:27 AM UTC

Hello @madhu1 ,

Indeed you need a transceiver. Example: ST3232

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
madhu1Author
Associate II
Feb 2, 2024 8:48 AM UTC

Can I use a voltage level shifter and then connect to UART pins of micro?

mƎALLEm
ST Technical Moderator
Feb 2, 2024 10:11 AM UTC

If you mean by "a voltage level shifter" to replace the transceiver, the answer is no.

This is the ranges for RS232 with negative voltage:

RS-232-Voltage-Levels.png

So please use a suitable transceiver.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.