Skip to main content
Champak Kundu
Associate II
December 4, 2023
Question

STM32G491REI6 got damage

We are using STM32G491REI6. PCB on which this microcontroller has been incorporated, developed by us.

In Inverter Application we are using this microcontroller.

When it is connected to operate inverter, every time the microcontroller IC got damaged. It got destroyed. That means no signals are coming from the microcontroller.

We need suggestions to resolve this issue.

This topic has been closed for replies.

1 reply

Peter BENSCH
ST Technical Moderator
December 4, 2023

It will be difficult to make suggestions to solve the problem if you do not provide details. All we know so far is that you are using an STM32G491REI6 and that no signals are coming from the microcontroller - which, by the way, is not a sufficient reason to assume that the microcontroller has been destroyed.

At least the schematics are important for an initial assessment; the firmware can be discussed afterwards.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.