Skip to main content
pazcal
Associate
August 26, 2022
Solved

STM32F779AI WLCSP 180 pins package layout examples

I would like to use the STM32F779AI, in WLCSP package. I did not find any application notes, or schematics or dev board for such MCU.

Is there some litterature or example, schematics, ... talking about layout rules, VIAs, etc... for the WLCSP-180 (pitch 0.4mm) package.

Thanks in advance

Pascal

This topic has been closed for replies.
FBLBest answer
ST Technical Moderator
August 29, 2022

Hi @pazcal​ 

Refer to this application note Getting started with STM32F7 Series MCU hardware development section 6.7 Recommendations for the WLCSP180 package then 8.5 WLCSP143 0.4 mm pitch design example

Also you can check the datasheet section 3 for more details about the pinout and package characteristics

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL

4 replies

Tesla DeLorean
Guru
August 26, 2022

TBH I think the people you should start with are the PCBA guys you work with, they'll have a lot more insight into the board, stack-up, solder mask, and via-in-pad type stuff they can work with, and which PCB vendors do a good job of fill/planarization, etc.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
pazcal
pazcalAuthor
Associate
August 31, 2022

Thanks for answer, but the question came from the PCBA Guys.

BR

paz

FBLBest answer
ST Technical Moderator
August 29, 2022

Hi @pazcal​ 

Refer to this application note Getting started with STM32F7 Series MCU hardware development section 6.7 Recommendations for the WLCSP180 package then 8.5 WLCSP143 0.4 mm pitch design example

Also you can check the datasheet section 3 for more details about the pinout and package characteristics

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL
pazcal
pazcalAuthor
Associate
August 31, 2022

Thanks for your answer. The A.N will help

BR

paz