Skip to main content
Roach
Associate II
May 14, 2021 7:30 PM UTC
Solved

STM32F769I-DISCO reference layout

Hello,

I'm planing to design a custom board using STM32F769 and I want to use the STM32F769I-DISCO as a reference but I didn't manage to find the PCB files in the CAD Resources section of the said product. There are only schematic packs, BOM and gerbers but no actual PCB file. I managed to download the whole Altium project for the NUCLEO-F767ZI around a year ago but it seems it's now the same deal with this one as well as with a lot of other products. Does anyone know how can I obtain some reference layout files for the STM32F769I-DISCO or why are they not available?

Thanks

This topic has been closed for replies.
Imen.DBest answer
ST Technical Moderator
May 21, 2021 11:13 AM UTC

Hi @Hrvoje Pu�?ak​ ,

You could find attached the migrated Altium project files of the STM32F769I-DISCO.

  

When your question is answered, please close this topic by choosing "Select as Best". This will help other users find that answer faster :smiling_face_with_smiling_eyes:.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks

3 replies

ST Technical Moderator
May 19, 2021 2:30 PM UTC

Hello @Hrvoje Pu�?ak​ ,

The PCB was not developed using Altium Designer but using another CAD tool and this is why it was initially not published on st.com.

Our hardware team are however working on a porting to Altium Designer,

I'll make sure to post any updates here as soon as I hear back from them, with either the original PCB document or possibly the migrated one to Altium Designer.

This AN4879 application note gives an overview of the USB peripherals implemented on STM32 MCUs, and provides hardware guidelines for PCB design, to ensure electrical compliance with the USB standards.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Imen.DBest answer
ST Technical Moderator
May 21, 2021 11:13 AM UTC

Hi @Hrvoje Pu�?ak​ ,

You could find attached the migrated Altium project files of the STM32F769I-DISCO.

  

When your question is answered, please close this topic by choosing "Select as Best". This will help other users find that answer faster :smiling_face_with_smiling_eyes:.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Hnos97
Visitor II
May 22, 2021 7:47 AM UTC

Bật mí kinh nghiệm soi cầu đ�? mi�?n Bắc – Chốt số dự đoán XSMB chắc ăn

Dự đoán kết quả xổ số mi�?n Bắc hôm nay ra con gì, chốt số đ�? soi cầu XSMB nhanh, chính xác hiện nay từ các bí quyết phân tích KQMB chắc ăn, bao trúng dưới đây:

  1. Cách chơi đ�? mi�?n Bắc là gì, trúng ăn bao nhiêu?

�?ánh đ�? là phương pháp ngư�?i chơi dự đoán trúng 2 số cuối của giải đặc biệt và tất nhiên tỷ lệ trúng sẽ cao hơn so với đánh lô. Cụ thể ngư�?i chơi nếu đặt cược với nhà cái chốt số đ�? nếu trúng tỷ lệ ăn là 1 ăn 70 – 80 lần tùy vào từng nhà cái.

Mặc dù đây là phương pháp chơi lô đ�? Xổ số mi�?n bắc ◀◀◀ CLICK không hợp pháp nhưng vẫn đảm bảo kết quả minh bạch bởi sựa vào kết quả xổ số kiến thiết mi�?n Bắc hàng ngày để làm căn cứ xác định trúng – trượt và sự hấp dẫn của tỷ lệ trúng, lãi khi chơi giúp trò chơi này vẫn luôn được nhi�?u ngư�?i ưa chuộng.

  1. Phương pháp soi cầu đ�? mi�?n Bắc hôm nay cực chuẩn xá

�?ể dự đoán số đ�? mi�?n Bắc hôm nay ra con gì chuẩn các bạn có thể dựa vào các thống kê KQXSMB kỳ trước đó để bắt cầu đ�?. Trong đó, có thể căn cứ vào các dấu hiệu KQXSMB ◀◀◀ BẤM XEM báo đ�? v�? hôm nay, ngày mai như sau:

- Nếu giải đặc biệt có số 0 nằm chính giữa giải (số thứ 3) thì đánh đ�? dàn chạm số 0. Tức là khi có dấu hiệu này các bạn nên ch�?n các đánh đ�? dàn với các cặp số có 2 chữ số trong đó có ít nhất 1 số là số 0.

- Soi cầu đ�? kép chuẩn xác: Nếu giải đặc biệt có dấu hiệu đ�? báo kép thì đừng quên bắt dàn đ�? kép nuôi khung 5 ngày tối đa nhé.

+ Nếu trong giải đặc biệt có 2 cặp số kép xuất hiện thì bắt dàn đ�? kép nuôi khung 5 kỳ liên tiếp. Ví dụ giải là 32299 thì có thấy có 2 cặp số kép là 22 và 99 nên đây là dấu hiệu đ�? báo kép.

+ Nếu giải đặc biệt có 2 số li�?n nhau giống nhau và tương tự giải nhất cũng xuất hiện cặp số kép thì có thể chốt số dự đoán đ�? kép hôm nay hoặc trong 5 ngày tới sẽ v�?. Vì vậy nên bắt dàn đ�? kép nuôi khung max 5 ngày tới.

Ngư�?i chơi có thể tham khảo các cầu số đẹp Xổ số kiến thiết mi�?n bắc ◀◀◀ TẠI �?ÂY hôm nay ra con gì chuẩn nhất dựa vào kết quả kỳ trước hoặc tham khảo các chia sẻ chốt số hàng ngày tại xsmb.me miễn phí mỗi ngày. Chúc các bạn có được cầu đẹp, chốt số chuẩn xác nhất!