Skip to main content
DVito.1
Associate
Oct 7, 2020 11:21 AM UTC
Solved

STM32F769I-Disco - no ST-Link detected

Hi guys,

I am new to STM32F769I-Disco and I‘ve got an error by trying to connect the STM to my pc.

In the STM32CubeIDE 1.4.0 I got the message: No-ST-Link detected

In ST-Link-Utility i got the same message.

ST-Link-Utility -> about: ST-Link-utility: v4.5.0; USBDriver.dll v5.1.2; ST-Link cli v3.5.

Additionaly no USB-Device is shown in my device-manger and the LD8(ST-Link connection) is blinking red. The display and so on is working well. I powered the board with usbhs and LD5 is green and LD6 is red.

Before I have worked with the same pc with STM32L0 and F1and both are ok. I’m able to connect in the IDE and in ST-Link-Utilities.

The ST-Link Debug version is 2.1.0.0.

I dont know what goes wrong.. I changed the usb cables and ports but no success.

Does anyone have an idea where the problem is ?

This topic has been closed for replies.
DVito.1
DVito.1Best answer
Associate
Oct 7, 2020 5:08 PM UTC

Thanks guys.

I got a new USB cable and changed the USB port again, but unfortunately no connection.

So I reinstalled the IDE and TouchGFX and now everything works. Maybe I did something wrong with the installation, I dont know

4 replies

Tesla DeLorean
Guru
Oct 7, 2020 11:49 AM UTC

Make sure you're not using charging cables.

​

Make sure you're connecting to the STLINK USB connector.

​

Make sure computer doesn't have policy settings regarding USB MSC, or AV software doing same.​

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Mike_ST
ST Technical Moderator
Oct 7, 2020 11:52 AM UTC

No idea,

But, please download STSW-LINK007 (ST-LINK upgrade utility) and

execute "ST-LinkUpgrade.exe -CheckVer" in a Windows Command Prompt.

CN3 has to be on "stlk" position.

if the ST-LINK chip is ok you should have a version number.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. 
Uwe Bonnes
Chief
Oct 7, 2020 1:47 PM UTC

Consider also bad cable and connectors.

DVito.1
DVito.1AuthorBest answer
Associate
Oct 7, 2020 5:08 PM UTC

Thanks guys.

I got a new USB cable and changed the USB port again, but unfortunately no connection.

So I reinstalled the IDE and TouchGFX and now everything works. Maybe I did something wrong with the installation, I dont know