Skip to main content
ADębs.1
Senior
Jun 16, 2021 9:22 PM UTC
Solved

STM32F746G-DISCO, STM32 ST-LINK Utility

STM32 STLINK Utility has stopped working. I'm sending the setting. What could be the reason?

[Settings]
File=
address=0x08000000
size=0x1000
data_width=4
connection=SWD
SwclkFrequency=15K
freq=8000
Connection_Mode=Normal
DebugInSleepMode=1
Reset_Mode=HWReset
Parallelism=32_Bits
AP_ID=0
RunAfterProge=1
FlashChecksum=0
SkipErase=0
SkipFlashProtection=0
trace.log=1
address1=0x08000000
address2=0x08010000
address3=0x080C0000
[LoopMode]
Device_ID=
MassErase=0
Program=1
Verify=0
OnChipverification=1
OBConfig=0
Run=0
FullChecksum=0
SkipErase=0
SkipProtection=0
OBVal=0000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000
[ExternalLoader]
ElfNumber=1
Elf1=C:\Program Files (x86)\STMicroelectronics\STM32 ST-LINK Utility\ST-LINK Utility\ExternalLoader\N25Q128A_STM32F746G-DISCO.stldr

Target: Detection Fail

Target Voltage: Detection Fail

Andrzej

This topic has been closed for replies.
Imen.DBest answer
ST Technical Moderator
Jun 17, 2021 9:18 AM UTC

Hello @Andrzej Dębski​ 

Check connection, USB cables, or maybe you have misplaced jumpers.

Try Connect under reset.

Check if you have problem with reset circuit and check pull BOOT0 low/high.

You can check if you have the same issue with other boards.

Please keep me informed about your progress on this issue.

Thanks 

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks

5 replies

Imen.DBest answer
ST Technical Moderator
Jun 17, 2021 9:18 AM UTC

Hello @Andrzej Dębski​ 

Check connection, USB cables, or maybe you have misplaced jumpers.

Try Connect under reset.

Check if you have problem with reset circuit and check pull BOOT0 low/high.

You can check if you have the same issue with other boards.

Please keep me informed about your progress on this issue.

Thanks 

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
ADębs.1
ADębs.1Author
Senior
Jun 17, 2021 10:01 AM UTC

The cable is good because I checked on the STM32F3DISCO (it has the same USB).

I am working with FLASH. It happened when the USB cable was disconnected / connected.

Could it be physical damage to the interface? How to check?

Is it possible to program the STM32F746G-DISCO via other USB?

Andrzej

ADębs.1
ADębs.1Author
Senior
Jun 24, 2021 3:39 PM UTC

I replaced U14 and T3 from the system where the PC-STM communication was. No change.

You wrote "check pull BOOT0 low / high" how to do it?

Andrzej