Skip to main content
FJB2069
Senior
January 29, 2025
Question

stm32F746g-disco custom board with Resistive lcd

My application requires a resistive lcd.  Is anyone familiar with trying to replace the existing capactive lcd with a resistive lcd?  

 

I have seen some resistive lcds with a similar 40 pin connection, but the I2C interface (pins 37-40) are the resistive signals.  Not sure if there is a resistive lcd with an i2C interface?

 

Appreciate any feedback.

 

This topic has been closed for replies.

4 replies

mƎALLEm
ST Technical Moderator
January 29, 2025

Hello,

There is a contradiction in the title: "stm32F746g-disco custom board", stm32F746g-disco is not a custom board. Could you please clarify this point so other community members could help you efficiently?

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
FJB2069
FJB2069Author
Senior
January 29, 2025

To clarify:  I am making a custom board based on the stm32F746-Disco, but I need the new board to work with a resistive lcd.

 

 

mƎALLEm
ST Technical Moderator
January 29, 2025

@FJB2069 wrote:

To clarify:  I am making a custom board based on the stm32F746-Disco, but I need the new board to work with a resistive lcd.


umm now it's clear.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Tesla DeLorean
Guru
January 29, 2025

The pool here is likely to be quite shallow, you'd do better talking to one of the LCD vendors/distributors about panels that meet your specific needs. If off-the-shelf versions with exact pinnage are not available you might need to create an interposer board.

Not sure the resistive controllers are particularly popular these days.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..