Skip to main content
WPong.1
Associate II
Dec 21, 2025 2:30 AM UTC
Question

STM32F746G-DISCO | Abnormal delay time at beginning

I created system_clock_initial function to config my board using PLL as system clock and running at 200MHz and also get APB1 timer at 100Mhz (for TIM5 delay function). See my code below. After that I create delay function from TIM5 and test with build-in LED when I upload my code to board and it begin to run, at beginning of time LED blink faster than delay time(1second) that I specify but after about 30 second LED blink properly with 1 second delay.

What should I fix it?

void system_clock_initial(void)
{
		/* Turn ON HSE oscillator */
		RCC->CR |= (RCC_CR_HSEON);
		while(!(RCC->CR & RCC_CR_HSERDY_Msk)){}

		/* Enable Power interface clock */
		RCC->APB1ENR |= (RCC_APB1ENR_PWREN);

		/* Enable Backup Domain Write Protection for Access Backup RTC & SDRAM */
		PWR->CR1 |= (PWR_CR1_DBP);

		/* Set flash period to 7 wait state */
		FLASH->ACR = (FLASH_ACR_LATENCY_7WS | FLASH_ACR_PRFTEN);

		/* PPRE1 Divide by 4 */
		RCC->CFGR = (RCC->CFGR & ~(RCC_CFGR_PPRE1_Msk)) | (RCC_CFGR_PPRE1_DIV4);

		/* PPRE2 Divide by 2 */
		RCC->CFGR = (RCC->CFGR & ~(RCC_CFGR_PPRE2_Msk)) | (RCC_CFGR_PPRE2_DIV2);

		/* RTCPRE Divide by 2 */
		RCC->CFGR = (RCC->CFGR & ~(RCC_CFGR_RTCPRE_Msk)) | (25 << RCC_CFGR_RTCPRE_Pos);

		/* Turn OFF PLL oscillator to config PLL*/
		RCC->CR &= ~(RCC_CR_PLLON);
		while((RCC->CR & (RCC_CR_PLLRDY_Msk))){}

		/* Select HSE as source for PLL */
		RCC->PLLCFGR |= (RCC_PLLCFGR_PLLSRC_HSE);

		/* Clear and set PLLM to 25 */
		RCC->PLLCFGR = (RCC->PLLCFGR & ~(RCC_PLLCFGR_PLLM_Msk)) | (PLLM_VAL << RCC_PLLCFGR_PLLM_Pos);

		/* Clear and set PLLN to 400 */
		RCC->PLLCFGR = (RCC->PLLCFGR & ~(RCC_PLLCFGR_PLLN_Msk)) | (PLLN_VAL << RCC_PLLCFGR_PLLN_Pos);

		/* Clear and set PLLP divide by 2 */
		RCC->PLLCFGR = (RCC->PLLCFGR & ~(RCC_PLLCFGR_PLLP_Msk));

		/* Clear and set PLLQ to 9 */
		RCC->PLLCFGR = (RCC->PLLCFGR & ~(RCC_PLLCFGR_PLLQ_Msk)) | (PLLQ_VAL << RCC_PLLCFGR_PLLQ_Pos);

		/* Turn ON PLL oscillator */
		RCC->CR |= (RCC_CR_PLLON);
		while((RCC->CR & (RCC_CR_PLLRDY_Msk)) == 0){}

		/* Config System Clock Switch as PLL */
		RCC->CFGR = (RCC->CFGR & ~(RCC_CFGR_SW_Msk)) | (RCC_CFGR_SW_PLL);
		while((RCC->CFGR & RCC_CFGR_SWS_PLL) == 0){}

}

2 replies

TDK
Dec 22, 2025 2:30 AM UTC

There's no mechanism in the chip that would cause the clock to spontaneously change after 30 seconds. I suspect the issue is in the code we're not seeing.

"If you feel a post has answered your question, please click ""Accept as Solution""."
mƎALLEm
ST Technical Moderator
Dec 22, 2025 8:33 AM UTC

Hello,

As you prefer the direct access to the register, better to use HAL and inspire from its register calls: sequence/values. 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.