Skip to main content
Associate
November 8, 2024
Question

STM32F446RE, SPI TX and Digilent ADP3450

There's a ghost in the machine!  Look at waveforms; CS randomly goes high during HAL_TransmitReceive.

 

uint8_t		EMIT_REG_I
( uint8_t R_I )
{
 uint8_t Ret_D;

 CS_0;
 DC_0;

 // SPI.TX
 Ret_D		= SPIx_Write ( R_I );

 CS_1;

 return		Ret_D;
}




uint8_t		EMIT_REG_V
( uint8_t R_V )
{
 uint8_t	Ret_D;

 CS_0;
 DC_1;

 Ret_D		=	SPIx_Write	( R_V );

 CS_1;

 return		Ret_D;
}



uint8_t		EMIT_REG_X
( uint8_t R_I, uint8_t R_V )
{
 EMIT_REG_I		( R_I );
 EMIT_REG_V		( R_V );

 return		0;
}


// TX Register Index and Register Index-'s Value
EMIT_REG_X		( 0xEB, 0x20 );

 

 

OS: Linux Ubuntu, Noble Numbat

WaveForms (3.23.4) and Adept installed from .deb package

 

Using Digilent ADP3450 to Measure SPI Protocol Logic Levels on an STM32F446RE.

SPI Baudrate is 4 MHz.

 

Digital GND on the ADP3450 is connected to GND on the STM32F446RE

DIO_0 is connected to SPI.CS on the STM32

DIO_1 is connected to SPI.SCK on the STM32

DIO_2 is conntected to SPI.MOSI on the STM32

DIO_3 is connected to SPI.MISO on the STM32

 

 

Using STM32 API HAL_SPI_TransmitReceive to TX Register Index and Register Value:

On Emit_X( 0xEB, 0x20 ) the logic waveform shows the following:

0xEB split apart, CS mysteriously goes high twice during TX

0x20 split apart, CS mysteriously goes high once during TX

 

What is the recommended fix?

This topic has been closed for replies.

1 reply

AtticusAuthor
Associate
November 10, 2024

Solved.

Spurious spikes on CS and DNC lines were caused by CrossTalk; forward and backward!