Skip to main content
FShah.1
Associate III
Oct 22, 2024 3:27 PM UTC
Question

STM32F446RE CRC mismatch

Hi, I am following a video to write a bootloader that transfers the application code serially into the STM32F446 controller. The video originally presents the STM32F7xx series controller, but I am applying it to the F4xxx series. I have modified the code as needed, such as assigning the proper flash areas for the bootloader and application code. See the GitHub link for this tutorial.

https://github.com/Embetronicx/STM32-Bootloader/tree/ETX_Bootloader_3.0/Bootloader_Example

This link also provides a PC tool that transfers the code from the host to the controller once the handshaking is complete.

What are the recommendations if I want to calculate the CRC32 on a PC that matches the CRC32 calculated on the STM32F446 using HAL_CRC_Calculate()?

My code gives 0x08b329c8 and host calculated CRC is 0x4e08bfb4?

This topic has been closed for replies.

10 replies

Tesla DeLorean
Guru
Oct 22, 2024 4:27 PM UTC

So posted three times on this topic.

STM32's standard algo operates on whole 32-bit words, in a right shifting word sense, which is not normative for little-endian platforms. See my code here

https://github.com/cturvey/RandomNinjaChef/blob/main/stm32crc.c

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
FShah.1
FShah.1Author
Associate III
Oct 22, 2024 4:35 PM UTC

@Tesla DeLorean 

Thank you for your response. I appreciate all the work done by community members, when I see a useful and understandable post, I add my question.

Should I use the code you linked on the host to calculate the CRC? Sorry if I'm asking a simple question!

Tesla DeLorean
Guru
Oct 22, 2024 5:47 PM UTC

Well, I'd start with your test pattern to affirm the calculation on PC vs the one you've got on the STM32

Most on-line calculators use more normative byte-wise computations.

On the F4 the CRC peripheral has a fixed form, which is 32-bit words. You can use the code to compute the equivalent for word aligned / word length multiples.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
FShah.1
FShah.1Author
Associate III
Dec 2, 2024 3:33 PM UTC

I checked the memory regions where the code is being written and identified an issue with how the data was being written to the flash memory—specifically, little-endian / big-endian issue. After addressing this, the application is now successfully loading and working.

Thanks for being responsive. I will reach out to you for assistance with other parts of the bootloader process during my development.

Thanks again,
FS

FShah.1
FShah.1Author
Associate III
Dec 2, 2024 10:31 PM UTC

Noted. I made these changes, and the code is still working. Please have a look and let me know if this is what you meant.

static void goto_application(void)
{

	
	printf("Gonna Jump to Application\r\n");

	// Set the Vector Table Offset Register (VTOR) to the address of the application
	SCB->VTOR = ETX_APP_FLASH_ADDR;
	// Get the application reset handler address
	void (*app_reset_handler)(void) = (void*)(*((volatile uint32_t*) (ETX_APP_FLASH_ADDR + 4U)));//Application starting address
	// Optionally turn off the LED
	HAL_GPIO_WritePin(GPIOD, GPIO_PIN_2, GPIO_PIN_RESET);
	__set_MSP(*(volatile uint32_t*) ETX_APP_FLASH_ADDR);
	/* Jump to application */
	app_reset_handler(); //call the app reset handler
}