Skip to main content
Gudgel.boB
Senior
June 1, 2021
Question

STM32F446 and ST-Link debugging all of a sudden stopped working with IAR 6.50 but STM32F334 still working

Hello comrades...

I have been using IAR 6.50 for a few years now with STM32F446VC 1-- pin uC and things have been working flawlessly. I also have more recently had a project using the STM32F334 controller and debugging just fine.

Last week, all of a sudden, the Flash loading and debugging stopped working with the STM32F446. This is with the ST-Link V2 pod . I have several pods and have tried this on 3 different computers (win 10 and win 7) with the same results. It just stopped working. Compiler is fine, just the debugging and IAR interface evidently. I have not changed any software.

When I DO get IAR to connect to the target, it will sit there saying Programming Flash Memory with no progression or timeout. It does not actually erase the chip. Sometimes I get the message that there is no target device detected. This is on 3 different computers it appears.

My STM32F334 project appears to work just fine with a STM32F3 Discovery board. Need to try the actual target with the pod.

ST-Link will program the STM32F446VC from the .hex file but stopping and starting the CORE through ST-Link sometimes crashes where the STM32F334 does not crash.

I tried a new project and the full project on more than one STM32446RE-Nucleo Eval boards and I get the same results.

 I also tried re-installing ST-Link drivers but nothing seems to have changed.

This really eludes me as to what might be happening. Any ideas or things to try ?

EDIT: I tried a small CubeMX program for a STM32F429ZI Discovery board and it also works fine in IAR and debugs and stops and starts etc.... It does use a different Flash EXE (.out file)

This issue must have to do with the FlashLoader software and different .OUT files that are used for flashing the parts. but I do not understand all I need to about these.

Debugging WiTHOUT download worked once on the 446 Nucleo times but otherwise says can't find the target device.

Thanks,

boB

This topic has been closed for replies.