Skip to main content
skrowten_hermit
Associate II
Jul 29, 2019 1:13 PM UTC
Solved

STM32F411RE vs STM32F446RE vs STM32F303RE ?

What exactly is the difference between Nucleo boards Nucleo-F303RE, Nucleo-F411RE and Nucleo-F446RE? To me, the data brief seems to suggest that they are the same. Can someone point out the difference? Is it okay if I buy any of these according to the availability? Have attached the Date brief for reference.

This topic has been closed for replies.
Amel NASRI
Amel NASRIBest answer
ST Technical Moderator
Aug 15, 2019 2:29 PM UTC

Hi @skrowten_hermit​ ,

You need to refer to UM1724.

-Amel

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.

4 replies

Tesla DeLorean
Guru
Jul 29, 2019 1:29 PM UTC

FLASH, RAM and SPEED?

F3 has different ADC performance.

You should probably look up the webpages for the micro-controller placed on each board.

If all that is unimportant for your unspecified application, any of them would suffice.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Bill Dempsey
Associate III
Jul 30, 2019 4:04 AM UTC

As stated above, there are speed & core ram/flash differences but also additional/different peripherals: CAN, UARTS, I2S, SPI (count), USB (type), etc...

There are nice pictorials of the boards over on the mbed.org website (color breakout of features on board) that might make it easier to understand

https://os.mbed.com/platforms/ST-Nucleo-F446RE/

https://os.mbed.com/platforms/ST-Nucleo-F303RE/

https://os.mbed.com/platforms/ST-Nucleo-F411RE/

skrowten_hermit
Associate II
Aug 1, 2019 5:38 AM UTC

This helps. I was looking for something like this. Thank you!

Amel NASRI
Amel NASRIBest answer
ST Technical Moderator
Aug 15, 2019 2:29 PM UTC

Hi @skrowten_hermit​ ,

You need to refer to UM1724.

-Amel

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.