Skip to main content
Senior
December 22, 2023
Solved

STM32F407G-DISC1 does not support virtual com, I cannot send data to PC via UART through virtual com

Hi All,

I can not send data from the board to the PC via UART. I can see that USART2 can be used as virtual com. But, when send data from board to the PC, I can not see anything on serial port, I use TeraTerm, Putty, Hercules. I thought the new version of STM32F407G-DISC1 board has this feature built in, but apparently it does not.

Can anyone help me with this please ?

This topic has been closed for replies.
Tesla DeLorean
Tesla DeLoreanBest answer
Guru
December 22, 2023

Correct, only later models had the firmware/parts for the ST-LINK/V2-1 (mbed) however the PCB does not support physically connectivity to any of the UARTs like later DISCO and NUCLEO models.

It could perhaps be wired, but honestly probably more of a headache. Perhaps use a cheap RPi-Pico as a USB-to-Serial, or use one of the NUCLEO-F429ZI, etc

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..

13 replies

STTwo-32
ST Technical Moderator
December 22, 2023

Hello @demir 

I think the replays in this link can help you. 

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Tesla DeLorean
Tesla DeLoreanBest answer
Guru
December 22, 2023

Correct, only later models had the firmware/parts for the ST-LINK/V2-1 (mbed) however the PCB does not support physically connectivity to any of the UARTs like later DISCO and NUCLEO models.

It could perhaps be wired, but honestly probably more of a headache. Perhaps use a cheap RPi-Pico as a USB-to-Serial, or use one of the NUCLEO-F429ZI, etc

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
pcb
Associate II
April 25, 2024

I too have an STM32F407G-DISC1.

I am successfully flashing code to it, and I know that the code

 

HAL_UART_Transmit(&huart2, (uint8_t *)message, strlen(message), 100);

 

runs, but I am not able to view my message by any means I have tried to cat ttyACM0, Putty, Serial Monitor plugin for VSCode.

Is it really so that serial communication is unavailable for this board? Doesn't that make it useless if you are integrating it into a system and want to (e.g.) read some sensor values such as the accelerometer?

Joachim SpangeHead in the embedded
demirAuthor
Senior
April 25, 2024

Thats right, you need the serial to usb converter.

demirAuthor
Senior
December 22, 2023

Hi @Tesla DeLorean AND @STTwo-32 

I have the STM32F407G-DISC1, MB997E. Isnt this supporting virtual com port ?

 

STTwo-32
ST Technical Moderator
December 22, 2023

No, this module include only  ST-LINK/V2-A wich is for SWD only without Virtual COM Port (VCP). But there is a workaround that allows you to retrofit the Virtual COM Port (VCP) for the ST-LINK/V2-A. You can find the workaround in the post mentionned on my first replay.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
demirAuthor
Senior
December 22, 2023

Could you please advise me some options that I can order which comes with Virtual Com Port ?

Thank you.

pcb
Associate II
April 26, 2024

Thank you @demir and @Tesla DeLorean!

I've been thinking there has to be a bug in my code, that 

HAL_UART_Transmit(&huart2, (uint8_t *)message, strlen(message), 100);

isn't the right way to print serial output. I've spent a few hours on this issue, and thanks to you I won't waste many more.

Why does the function HAL_UART_Transmit even exist for the STM32F407G-DISC1?
If it does work, it shouldn't exist, or perhaps the editor (I use VSCode) should at least display a warning.

Joachim SpangeHead in the embedded