Skip to main content
Associate
August 20, 2024
Solved

STM32F407 Discovery board UART problem

Hello,

I am new to STM32 and need help with UART, please. I have been trying to transfer data with my STM32F407 Discovery Board to the console for a few days. I am using the STM32CUBE IDE, which has a special Command Shell Console to read data from serial ports. Unfortunately, the Command Shell Console remains empty when running the code. I also used 'screen' as an alternative, as I am working under macOS, but this console also stays empty. I have paid attention to the baud rates (115200) and have also tried various clock frequencies. What could be other sources of error that cause no output? I have also posted the code to demonstrate my simple project.

I am very happy about any help and suggestions!

 

 

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file : main.c
 * @brief : Main program body
 ******************************************************************************
 * @attention
 *
 * Copyright (c) 2024 STMicroelectronics.
 * All rights reserved.
 *
 * This software is licensed under terms that can be found in the LICENSE file
 * in the root directory of this software component.
 * If no LICENSE file comes with this software, it is provided AS-IS.
 *
 ******************************************************************************
 */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"
#include <string.h>

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */

/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
#define TIMEOUT 100
/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/
I2S_HandleTypeDef hi2s3;
UART_HandleTypeDef huart2;

/* USER CODE BEGIN PV */

/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_I2S3_Init(void);
static void MX_USART2_UART_Init(void);
/* USER CODE BEGIN PFP */

/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */

/* USER CODE END 0 */

/**
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{

 /* USER CODE BEGIN 1 */
 char msg[] = "Hello World!\n";
 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */
 SystemClock_Config();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_I2S3_Init();
 MX_USART2_UART_Init();
 /* USER CODE BEGIN 2 */

 /* USER CODE END 2 */

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
	HAL_UART_Transmit(&huart2, (const uint8_t*) msg, strlen(msg), 100);
	HAL_Delay(1000);
 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */

 }
 /* USER CODE END 3 */
}

/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 /** Configure the main internal regulator output voltage
 */
 __HAL_RCC_PWR_CLK_ENABLE();
 __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);

 /** Initializes the RCC Oscillators according to the specified parameters
 * in the RCC_OscInitTypeDef structure.
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
 RCC_OscInitStruct.HSEState = RCC_HSE_ON;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
 RCC_OscInitStruct.PLL.PLLM = 4;
 RCC_OscInitStruct.PLL.PLLN = 96;
 RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV6;
 RCC_OscInitStruct.PLL.PLLQ = 4;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK)
 {
 Error_Handler();
 }
}

/**
 * @brief I2S3 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_I2S3_Init(void)
{

 /* USER CODE BEGIN I2S3_Init 0 */

 /* USER CODE END I2S3_Init 0 */

 /* USER CODE BEGIN I2S3_Init 1 */

 /* USER CODE END I2S3_Init 1 */
 hi2s3.Instance = SPI3;
 hi2s3.Init.Mode = I2S_MODE_MASTER_TX;
 hi2s3.Init.Standard = I2S_STANDARD_PHILIPS;
 hi2s3.Init.DataFormat = I2S_DATAFORMAT_16B;
 hi2s3.Init.MCLKOutput = I2S_MCLKOUTPUT_ENABLE;
 hi2s3.Init.AudioFreq = I2S_AUDIOFREQ_96K;
 hi2s3.Init.CPOL = I2S_CPOL_LOW;
 hi2s3.Init.ClockSource = I2S_CLOCK_PLL;
 hi2s3.Init.FullDuplexMode = I2S_FULLDUPLEXMODE_DISABLE;
 if (HAL_I2S_Init(&hi2s3) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN I2S3_Init 2 */

 /* USER CODE END I2S3_Init 2 */

}

/**
 * @brief USART2 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_USART2_UART_Init(void)
{

 /* USER CODE BEGIN USART2_Init 0 */

 /* USER CODE END USART2_Init 0 */

 /* USER CODE BEGIN USART2_Init 1 */

 /* USER CODE END USART2_Init 1 */
 huart2.Instance = USART2;
 huart2.Init.BaudRate = 115200;
 huart2.Init.WordLength = UART_WORDLENGTH_8B;
 huart2.Init.StopBits = UART_STOPBITS_1;
 huart2.Init.Parity = UART_PARITY_NONE;
 huart2.Init.Mode = UART_MODE_TX_RX;
 huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE;
 huart2.Init.OverSampling = UART_OVERSAMPLING_16;
 if (HAL_UART_Init(&huart2) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN USART2_Init 2 */

 /* USER CODE END USART2_Init 2 */

}

/**
 * @brief GPIO Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_GPIO_Init(void)
{
 GPIO_InitTypeDef GPIO_InitStruct = {0};
/* USER CODE BEGIN MX_GPIO_Init_1 */
/* USER CODE END MX_GPIO_Init_1 */

 /* GPIO Ports Clock Enable */
 __HAL_RCC_GPIOE_CLK_ENABLE();
 __HAL_RCC_GPIOC_CLK_ENABLE();
 __HAL_RCC_GPIOH_CLK_ENABLE();
 __HAL_RCC_GPIOA_CLK_ENABLE();
 __HAL_RCC_GPIOB_CLK_ENABLE();
 __HAL_RCC_GPIOD_CLK_ENABLE();

 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(CS_I2C_SPI_GPIO_Port, CS_I2C_SPI_Pin, GPIO_PIN_RESET);

 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(OTG_FS_PowerSwitchOn_GPIO_Port, OTG_FS_PowerSwitchOn_Pin, GPIO_PIN_SET);

 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(GPIOD, GPIO_PIN_8|GPIO_PIN_9|LD4_Pin|LD3_Pin
 |LD5_Pin|LD6_Pin|Audio_RST_Pin, GPIO_PIN_RESET);

 /*Configure GPIO pin : CS_I2C_SPI_Pin */
 GPIO_InitStruct.Pin = CS_I2C_SPI_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(CS_I2C_SPI_GPIO_Port, &GPIO_InitStruct);

 /*Configure GPIO pin : OTG_FS_PowerSwitchOn_Pin */
 GPIO_InitStruct.Pin = OTG_FS_PowerSwitchOn_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(OTG_FS_PowerSwitchOn_GPIO_Port, &GPIO_InitStruct);

 /*Configure GPIO pin : PDM_OUT_Pin */
 GPIO_InitStruct.Pin = PDM_OUT_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 GPIO_InitStruct.Alternate = GPIO_AF5_SPI2;
 HAL_GPIO_Init(PDM_OUT_GPIO_Port, &GPIO_InitStruct);

 /*Configure GPIO pin : B1_Pin */
 GPIO_InitStruct.Pin = B1_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_EVT_RISING;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(B1_GPIO_Port, &GPIO_InitStruct);

 /*Configure GPIO pins : SPI1_SCK_Pin SPI1_MISO_Pin SPI1_MOSI_Pin */
 GPIO_InitStruct.Pin = SPI1_SCK_Pin|SPI1_MISO_Pin|SPI1_MOSI_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 GPIO_InitStruct.Alternate = GPIO_AF5_SPI1;
 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

 /*Configure GPIO pin : BOOT1_Pin */
 GPIO_InitStruct.Pin = BOOT1_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(BOOT1_GPIO_Port, &GPIO_InitStruct);

 /*Configure GPIO pin : CLK_IN_Pin */
 GPIO_InitStruct.Pin = CLK_IN_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 GPIO_InitStruct.Alternate = GPIO_AF5_SPI2;
 HAL_GPIO_Init(CLK_IN_GPIO_Port, &GPIO_InitStruct);

 /*Configure GPIO pins : PD8 PD9 LD4_Pin LD3_Pin
 LD5_Pin LD6_Pin Audio_RST_Pin */
 GPIO_InitStruct.Pin = GPIO_PIN_8|GPIO_PIN_9|LD4_Pin|LD3_Pin
 |LD5_Pin|LD6_Pin|Audio_RST_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);

 /*Configure GPIO pin : VBUS_FS_Pin */
 GPIO_InitStruct.Pin = VBUS_FS_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(VBUS_FS_GPIO_Port, &GPIO_InitStruct);

 /*Configure GPIO pins : OTG_FS_ID_Pin OTG_FS_DM_Pin OTG_FS_DP_Pin */
 GPIO_InitStruct.Pin = OTG_FS_ID_Pin|OTG_FS_DM_Pin|OTG_FS_DP_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 GPIO_InitStruct.Alternate = GPIO_AF10_OTG_FS;
 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

 /*Configure GPIO pin : OTG_FS_OverCurrent_Pin */
 GPIO_InitStruct.Pin = OTG_FS_OverCurrent_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_INPUT;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(OTG_FS_OverCurrent_GPIO_Port, &GPIO_InitStruct);

 /*Configure GPIO pins : Audio_SCL_Pin Audio_SDA_Pin */
 GPIO_InitStruct.Pin = Audio_SCL_Pin|Audio_SDA_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_OD;
 GPIO_InitStruct.Pull = GPIO_PULLUP;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 GPIO_InitStruct.Alternate = GPIO_AF4_I2C1;
 HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);

 /*Configure GPIO pin : MEMS_INT2_Pin */
 GPIO_InitStruct.Pin = MEMS_INT2_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_EVT_RISING;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(MEMS_INT2_GPIO_Port, &GPIO_InitStruct);

/* USER CODE BEGIN MX_GPIO_Init_2 */
/* USER CODE END MX_GPIO_Init_2 */
}

/* USER CODE BEGIN 4 */
int _write(int file, char *ptr, int len)
{
 (void)file;
 int DataIdx;

 for (DataIdx = 0; DataIdx < len; DataIdx++)
 {
 ITM_SendChar(*ptr++);
 }
 return len;
}
/* USER CODE END 4 */

/**
 * @brief This function is executed in case of error occurrence.
 * @retval None
 */
void Error_Handler(void)
{
 /* USER CODE BEGIN Error_Handler_Debug */
 /* User can add his own implementation to report the HAL error return state */
 __disable_irq();
 while (1)
 {
 }
 /* USER CODE END Error_Handler_Debug */
}

#ifdef USE_FULL_ASSERT
/**
 * @brief Reports the name of the source file and the source line number
 * where the assert_param error has occurred.
 * @PAram file: pointer to the source file name
 * @PAram line: assert_param error line source number
 * @retval None
 */
void assert_failed(uint8_t *file, uint32_t line)
{
 /* USER CODE BEGIN 6 */
 /* User can add his own implementation to report the file name and line number,
 ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
 /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */

 

 

This topic has been closed for replies.
KnarfB
KnarfBBest answer
Super User
August 20, 2024

This board has ST-LINK/V2-A and there is no USART2 to host connection unless you solder one.

See this post: Solved: STM32F407G-DISC1 ST-LINK/V2-A with virtual COM p... - STMicroelectronics Community

hth

KnarfB 

4 replies

KnarfB
KnarfBBest answer
Super User
August 20, 2024

This board has ST-LINK/V2-A and there is no USART2 to host connection unless you solder one.

See this post: Solved: STM32F407G-DISC1 ST-LINK/V2-A with virtual COM p... - STMicroelectronics Community

hth

KnarfB 

Andrew Neil
Super User
August 20, 2024

As well as the thread linked by @KnarfB, see also:

https://community.st.com/t5/stm32cubeide-mcus/serial-monitor-not-working/m-p/695888/highlight/true#M28875

which also explains that you have to make some connections manually.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Tesla DeLorean
Guru
August 20, 2024

As I recall the STM32F4-DIS-BB used USART6 to get an RS232 serial port out.

It never supported the mbed VCP method, although the DISC1 board did get the STM32F103 changed, and the newer firmware, the plumbing for the pins never got wired.

Use SWD / SWV method, that worked as I recall, might need a solder-bridge (SB) on the PB3 / SWO pin.

 

https://www.st.com/en/evaluation-tools/stm32f4dis-ext.html

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Associate
August 20, 2024

Would be great just using jumpers to wire the pins..  

I used SWV now. Big thank you for mentioning it. It's the much more easier solution here.