Skip to main content
Associate II
April 11, 2024
Solved

STM32F3DISCOVERY UART communication with a PC

Hi,

I'm trying to create my custom UART firmware on STM32F3DISCOVERY board. Since I wrote the Transmit part of the driver and I verified that it continuously writes words to the USART_TDR register, I was going to check whether the UART messages are actually outputted from the MCU pins.

So far the plan is just to continuously spam some messages via PC4 pin to the on-board ST-link debugger. Since I know that I have a PCB version C, the on-board debugger should be of version ST-LINK/V2-B, meaning that it has virtual COM port interface on USB.

My main question is, do I understand it correctly, that just by sending  some UART messages from the MCU pin PC4 to debugger, the virtual COM port of the debugger shall automatically re-send these messages to a PC, where I should be able to read them with some UART compatible terminal (e.g. PuTTy, Serial Debug Assistant, etc.)?

Or am I missing some more steps? Like, are there some other steps involved to make the on-board debugger to re-send UART messages via USB COM port?

This topic has been closed for replies.
Pavel A.
Pavel A.Best answer
April 11, 2024

@pav_ivanovsAnd be sure to set the correct baudrate, parity etc. on both STM32 and PC sides. This is critical.

> the on-board debugger should be of version ST-LINK/V2-B, meaning that it has virtual COM port interface on USB.

This is very easy to see. Open the device manager and plug the board into USB port. Two devices should appear: the ST-LINK and VCP UART. A disk device can come too. If you don't see the UART, the ST-LINK does not support it.

5 replies

Andrew Neil
Super User
April 11, 2024

@pav_ivanovs wrote:

do I understand it correctly, that just by sending  some UART messages from the MCU pin PC4 to debugger, the virtual COM port of the debugger shall automatically re-send these messages to a PC, where I should be able to read them with some UART compatible terminal (e.g. PuTTy, Serial Debug Assistant, etc.)?


Yes.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Pavel A.
Pavel A.Best answer
April 11, 2024

@pav_ivanovsAnd be sure to set the correct baudrate, parity etc. on both STM32 and PC sides. This is critical.

> the on-board debugger should be of version ST-LINK/V2-B, meaning that it has virtual COM port interface on USB.

This is very easy to see. Open the device manager and plug the board into USB port. Two devices should appear: the ST-LINK and VCP UART. A disk device can come too. If you don't see the UART, the ST-LINK does not support it.

Associate II
April 12, 2024

pav_ivanovs_0-1712902998459.png

When I plug my STM32F3DISCOVERY board, I get 3 new devices: ST-Link Debug, USB Composite Device and STLink Virtual COM port (COM3). Shouldn't the general Virtual COM Port be capable of transmitting UART messages, or do I need exactly VCP UART?

Karl Yamashita
Principal
April 12, 2024

COM3 is your VCP.

 

Putty, Docklight or even the built in serial terminal that STM32CubeIDE has will work to receive from the MCU. 

 

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source
Associate II
April 12, 2024

Alright, thanks everyone for the answers, after some debugging, I made it to work just as you said.