Skip to main content
BLu.397
Visitor II
October 24, 2019
Solved

STM32F030C6 breakpoint setting does NOT work on STM32CubeIDE using ST-link V2. Is it a BUG or setup issue? and how?

When I hit Debug. System stops at first line of main() as intended. However no matter how I setup any breakpoints on the rest code, and hit Resume(F8) button. The code never stops on those breakpoint. even though I am 100% sure those breakpointed line code got run already. and if I hit suspend. the code stops normally. Also step into or over works normally. ( I am sure that the number of breakpoints I setup is less than 4) I checked log file of st link GDB server. I did not see any breakpoint setting command sent to the debugger via the SWD. Is this a software bug of CubeIDE? I saw some youtube video. it shows the breakpoint works fine. Could anyone give me some hint. I stuck on this issue for two days. :(

This topic has been closed for replies.
Mavoodoo
MavoodooBest answer
Associate
March 26, 2020

Hi BLu.397,

Have you made sure breakpoints aren't globally disabled? There is an option under Run -> Skip All Breakpoints Ctrl+Alt+B

I'm using Cube IDE 1.3.0

Cheers...

10 replies

David SIORPAES
ST Employee
October 24, 2019

Have you tried setting no optimizations (-O0) ?

Mavoodoo
MavoodooBest answer
Associate
March 26, 2020

Hi BLu.397,

Have you made sure breakpoints aren't globally disabled? There is an option under Run -> Skip All Breakpoints Ctrl+Alt+B

I'm using Cube IDE 1.3.0

Cheers...

DFres.1
Associate
March 16, 2021

Solved my problem, thanks!

ST Technical Moderator
March 17, 2021

Hi @DFres.1​ ,

Did the solution proposed by @David SIORPAES​  or @Mavoodoo​ solve your problem?

Please mark the post that helped you by clicking on the "Select as Best" button.

Otherwise, share your solution and mark it as a Best Answer.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
GCANG.1
Visitor II
July 20, 2021

Hi all, I'm same issue. Please, could you help me?

Associate III
April 26, 2024

Confirm - the answer of @Mavoodoo solved this problem on my IDE 1.14.1. A huge thanks.