Skip to main content
DrOnline
Associate II
May 21, 2022
Solved

STM32CubeProgrammer with STLINK-V3SET fails to program STM32L4P5ZGT6P about 90% of time

I've spend a lot of time on this, and I am out of ideas.

I'm a test engineer, and I have a bunch of boards my customer wants programmed.

I run the command STM32_Programmer_CLI.exe -c port=swd -w "C:\FW.hex" -v -q but it will fail a lot. I wrote 90% in the title, but it's so odd, because once it works, which may take 10 attempts, it will most likely work again and again if I just keep running that command. I have tried multiple computers, and they all exhibit this behaviour. The customer says they always manage to program the boards with zero issue whatsoever.

It used to work just fine, when I programmed dozens of these boards last year. Maybe the programmer is broken. If I could just buy a new V3, I would, but nowhere is in stock. If anybody knows how I can get one, please give me advice. This is my only unit.

C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin>STM32_Programmer_CLI.exe -c port=swd -w "C:\FW.hex" -v -q
 -------------------------------------------------------------------
 STM32CubeProgrammer v2.10.0
 -------------------------------------------------------------------
 
ST-LINK SN : 003300413438511134313939
ST-LINK FW : V3J7M2B4S1
Board : STLINK-V3SET
Voltage : 3.26V
Error: No STM32 target found!
2nd connect tentative with a lower frequency (8MHz)
ST-LINK SN : 003300413438511134313939
ST-LINK FW : V3J7M2B4S1
Board : STLINK-V3SET
Voltage : 3.27V
Error: No STM32 target found!
 
C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin>STM32_Programmer_CLI.exe -c port=swd -w "C:\FW.hex" -v -q
 -------------------------------------------------------------------
 STM32CubeProgrammer v2.10.0
 -------------------------------------------------------------------
 
ST-LINK SN : 003300413438511134313939
ST-LINK FW : V3J7M2B4S1
Board : STLINK-V3SET
Voltage : 3.28V
SWD freq : 24000 KHz
Connect mode: Normal
Reset mode : Software reset
Device ID : 0x471
Revision ID : Rev Z
Device name : STM32L4Pxxx/STM32L4Qxxx
Flash size : 1 MBytes
Device type : MCU
Device CPU : Cortex-M4
BL Version : --
Debug in Low Power mode enabled
 
 
 
Memory Programming ...
Opening and parsing file: FW.hex
 File : FW.hex
 Size : 280.17 KB
 Address : 0x08020000
 
 
Erasing memory corresponding to segment 0:
Erasing internal memory sectors [32 102]
Download in Progress:
 
 
File download complete
Time elapsed during download operation: 00:00:07.190
 
 
 
Verifying ...
 
 
 
 
Download verified successfully
 
 
 
C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin>

Any advice would be HIGHLY appreciated.

This topic has been closed for replies.
Piranha
PiranhaBest answer
Principal III
May 21, 2022

Connect mode: Under reset

Reset mode: Hardware reset

6 replies

Tesla DeLorean
Guru
May 21, 2022

Current firmware

Is the reset pin connected in your use case?

Connect under reset.

Reduced connection speed.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
DrOnline
DrOnlineAuthor
Associate II
May 21, 2022

OK, I've upgraded FW on the V3 from:

V3J7M2B4S1

to:

V3J9M3B5S1

STM32CubeProgramer is v 2.10.0 (latest)

Yes, STM32_nRST is connected, I just checked with an ohmmeter that it goes from the V3 pin to the header of the board properly.

When you say connect under reset, you mean as a part of my command line?

So I just tried again without changing the speed, and it failed on the first try, then succeeded on the second. Reducing to freq=100 worked on first try, but that might be the phenomenon I described before where if it works once it tends to work multiple times over. Let me try with freq=500 and go through a few units. Thank you for your advice.

DrOnline
DrOnlineAuthor
Associate II
May 21, 2022

I'm afraid the problem still persists. I retry multiple times to get it through.

I have also tried multiple cables between the DUT (the customer's board), and the V3 programmer, and it appears to make no difference.

Piranha
PiranhaBest answer
Principal III
May 21, 2022

Connect mode: Under reset

Reset mode: Hardware reset

DrOnline
DrOnlineAuthor
Associate II
May 21, 2022

I've left work. Will try this on Monday. Thank you. ​

DrOnline
DrOnlineAuthor
Associate II
May 23, 2022

Hi, reset=HWrst seems to have done the trick. I have removed the freq=500 line so it uses 8MHz now and it has worked flawlessly for three boards in a row, which was impossible before. Thank you both very much. Extremely good help, and I appreciate it a lot.

So.... man.. I spent so much time on this problem. The default setting for reset appears to be SWrst. That did not work. How would I ever find that out on my own? What is the general advice for SWrst vs HWrst? Why does HWrst work so well?