Skip to main content
peter__
Associate
Dec 5, 2019 8:56 AM UTC
Solved

STM32CubeIDE 1.1.0 does not offer Segger J-LINK debug probe in debug configurations

I freshly installed STM32CubeIDE (with J-LINK and ST-LINK selected during install) and created a new projekt. When trying to create a debug configuration Segger J-LINK is not selectable as debug adapter - only ST-Link.

Tried on Windows and Linux.

Also tried to install Segger JLINK tools afterwards with no effect.

Best,

P

This topic has been closed for replies.
Markus GIRDLAND
Markus GIRDLANDBest answer
ST Employee
Dec 5, 2019 10:17 AM UTC

It's fixed internally and will be part of the next release.

4 replies

hansd56
Senior
Dec 5, 2019 9:03 AM UTC

Hi, there was an answer from an ST employe not too long ago. Apperently, because of H7 dual core mcu's the J-Link option has been taken out for H7. I just had a look and It is still present for F7 etc.

peter__
peter__Author
Associate
Dec 5, 2019 10:03 AM UTC

OK - I'm using an STM32H7 indeed .. but a single-core version.

Would be great if JLINK support was added for these MCUs.

Markus GIRDLAND
Markus GIRDLANDBest answer
ST Employee
Dec 5, 2019 10:17 AM UTC

It's fixed internally and will be part of the next release.

Cartu38 OpenDev
Graduate II
Jan 10, 2020 9:21 AM UTC

Solved if STM32CubeIDE 1.2.0 release according to me