Skip to main content
Linas L
Senior
June 21, 2019
Question

STM32753 and STM32H747 compatibility in TFBGA240+25

Hi.

Just find out about dual core version of processor i like, and i would definitely want it to use in my board, since it offers some good advantages over single core.

But it is a bit hard to understand if STM32H753XI is compatible .

"The TFBGA240+25 ballout is compatible with STM32H7x3 devices, except for a few

I/O balls as shown in Figure 2."

It looks like it can run on internal LDO, since i don't care about power usage with 24V 10A power supply.

So that means i just keep my VCAPS and that's it ? since SMPS looks like just source for bypassing internal LDO.

Is this correct ?

This topic has been closed for replies.

1 reply

Amel NASRI
ST Technical Moderator
July 5, 2019

Hi @Linas L​ ,

In theory, yes they are compatible.

But to avoid side effects & to make sure that your assumption is correct, please refer to AN4938: Getting started with STM32H74xI/G and STM32H75xI/G hardware development.

Another important application note to check is AN5036: Thermal management guidelines for STM32 applications.

-Amel

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.