Skip to main content
Associate II
Oct 28, 2025 8:04 AM UTC
Solved

STM320U LPUART2 not working after waking up from the STOP0/ Sleep Mode.

Hello Everyone,

I am currently using LPUART2 for communication between an MCU (STM32U031) and an MPU (Application Processor).
Configuration parameters:

  • Baud rate: 9600
  • Stop bits: 1
  • Parity: None
  • Data bits: 8

Description:

Data exchange between MCU and MPU works perfectly when both devices are operating in normal power mode (i.e., not in sleep or stop modes). However, I am facing an issue when both MCU and MPU wake up from sleep/stop mode.

 

After wake-up ,The MCU is unable to receive data from the MPU, even though the MPU continues transmitting data. No IRQ handler is triggered on the MCU side.

Additional Details:

  1. I deinitialize the LPUART before entering sleep/stop mode.
  2. I reinitialize it immediately after wake-up.

Scenarios Tested:

Only MPU enters sleep (MCU remains active): After MPU wake-up, communication works perfectly.

Both MPU and MCU enter sleep: After wake-up, communication fails (MCU doesn’t receive data).


Observation:

It seems that the issue is related to LPUART behavior during low power transitions, since everything works fine when only the MPU performs sleep/wake operations and the MCU remains awake.


Please help identify if there is missing configuration or specific setup required for LPUART in low power modes?

I am open to share the source code and any other information.

Gyessine
GyessineBest answer
ST Technical Moderator
Oct 28, 2025 3:44 PM UTC

hello @suresh kumar1 

Do you get the same issue when you try using LPUART1?

You can refer to the provided examples for guidance : example 1,example 2

BR
Gyessine

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

2 replies

Gyessine
GyessineBest answer
ST Technical Moderator
Oct 28, 2025 3:44 PM UTC

hello @suresh kumar1 

Do you get the same issue when you try using LPUART1?

You can refer to the provided examples for guidance : example 1,example 2

BR
Gyessine

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Associate II
Jan 29, 2026 9:04 AM UTC

Hi, 
I know I am a bit late to this, but i am facing the same issue. It works fine with LPUART1 (the ST example) but breaks for LPUART2 (and even observed with LPUART3). I have made a detailed post here
Any solution or explanation for this would be much appreciated.