Skip to main content
Associate
Nov 18, 2025 5:01 PM UTC
Solved

STM32 Nucleo-H723ZG PA11&PA12 not working? (GPIO & FDCAN)

Dear Community,

I am using a Nucleo-H723ZG for my uni project and im running into issues with the PA11 & PA12 Pins.

I want to use them for FDCAN1 and I have verified that my code works.

 

No matter in what way i try to use these two pins the dont output.

if I switch to FDCAN2 with the same code and simply switch all instances of &hfdcan1 to &hfdcan2 i can read the signals with an scope and a can2usb adapter and get the right values.

 

I also tried to select just the mcu instead of the board because i read that sometimes USB_OTG messes with things but no luck.

Lastly i tried with another brand new Nucleo-H723ZG but also here no output on PA11 & PA12 whatsoever.

Not even in GPIO-Mode.

 

Do I have to turn something specific of?

I attached the full project.

 

Kind regards

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Nov 18, 2025 5:08 PM UTC

Hello @NeverRest and welcome to the community;

mALLEm_0-1763485439538.png

PA11 & PA12 are used by the USB on the board.

Meanwhile you can play with the solder bridges according to the board schematic:

To remove SB21 and SB22 to disconnect these IOs from the USB hardware part:

mALLEm_1-1763485582523.png

and solder SB16 and SB17 to connect them to CN12 connector: 

mALLEm_3-1763485735913.png

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

4 replies

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Nov 18, 2025 5:08 PM UTC

Hello @NeverRest and welcome to the community;

mALLEm_0-1763485439538.png

PA11 & PA12 are used by the USB on the board.

Meanwhile you can play with the solder bridges according to the board schematic:

To remove SB21 and SB22 to disconnect these IOs from the USB hardware part:

mALLEm_1-1763485582523.png

and solder SB16 and SB17 to connect them to CN12 connector: 

mALLEm_3-1763485735913.png

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
NeverRestAuthor
Associate
Nov 18, 2025 5:26 PM UTC

First of all thank you very much for your quick & detailed answer.

I have just one question.

The Nucleo board has two usb ports.

Which of these two does this affect and will this affect my abillity to flash code to the board via usb?

 

Kind regards

TDK
Nov 18, 2025 6:00 PM UTC

It affects the USER USB port. It does not affect your ability to flash and debug the chip with ST-Link.

"If you feel a post has answered your question, please click ""Accept as Solution""."
NeverRestAuthor
Associate
Nov 18, 2025 7:03 PM UTC

Okay thank you for the clarification.

You two guys are my heroes.