Skip to main content
PMoop.1
Associate
March 19, 2021
Question

Stm32 nucleo-f412zg powered externally acts weird

I'm using Stm32f4 nucleo-f412z g for a test fixture kind of setup. After loading the firmware I want to keep the eval board in a box and power it externally with a power brick and usb. But when I do this, it doesn't work with the firmware I uploaded. It behaves weird, has anyone come across a similar issue or is there a solution for this??

This topic has been closed for replies.

3 replies

Ozone
Principal
March 19, 2021

Check your "power brick" output.

Some have rather high voltages without load.

And others collpase near the current limit.

PMoop.1
PMoop.1Author
Associate
March 19, 2021

Connected to a power supply, brought down input voltage to 3V, there's no difference. It draws around 60mA of current. @Ozone​ 

Ozone
Principal
March 22, 2021

Well, 60mA doesn't sound too much.

I once had a board with a LCD display that behaved strangely when powered by the integrated debug pod via USB.

Only with an external power supply it worked correctly.

I would still check the idle voltage of your power brick, and the temperature of all reachable chips at least with your fingers.

And try debugging.

Either an unreliable initialisation (clock/Flash settings). Or, if you loose the debugging connection at a consistent location, related to some peripheral.