Skip to main content
MS.23
Associate II
Aug 18, 2023 6:46 AM UTC
Solved

STM32 dual channel ADC

I am trying to read ADC from two channels without using DMA. For that I use this code:

 

/* USER CODE BEGIN 0 */
uint16_t ADC_VAL[2];

void ADC_Select_CH1(void)
{
    ADC_ChannelConfTypeDef sConfig = {0};
 
    sConfig.Channel = ADC_CHANNEL_0;
    sConfig.Rank = ADC_REGULAR_RANK_1;
    sConfig.SamplingTime = ADC_SAMPLETIME_1CYCLE_5;
    if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
    {
      Error_Handler();
    }
}

void ADC_Select_CH2(void)
{
    ADC_ChannelConfTypeDef sConfig = {0};
 
    sConfig.Channel = ADC_CHANNEL_1;
    sConfig.Rank = ADC_REGULAR_RANK_2;
    if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
    {
      Error_Handler();
    }
}
/* USER CODE END 0 */

/**
  * @brief  The application entry point.
  * @retval int
  */
int main(void)
{
  /* MCU Configuration--------------------------------------------------------*/

  /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
  HAL_Init();

  /* Configure the system clock */
  SystemClock_Config();

  /* Initialize all configured peripherals */
  MX_GPIO_Init();
  MX_USART2_UART_Init();
  MX_ADC1_Init();

  /* Infinite loop */
  /* USER CODE BEGIN WHILE */
  while (1)
  {
    /* USER CODE END WHILE */

    /* USER CODE BEGIN 3 */
          //1st channel ADC conversion
          ADC_Select_CH1();
          HAL_ADC_Start(&hadc1);
          HAL_ADC_PollForConversion(&hadc1, 1000);
          ADC_VAL[0] = HAL_ADC_GetValue(&hadc1);
          HAL_ADC_Stop(&hadc1);
 
          //2nd channel ADC conversion
          ADC_Select_CH2();
          HAL_ADC_Start(&hadc1);
          HAL_ADC_PollForConversion(&hadc1, 1000);
          ADC_VAL[1] = HAL_ADC_GetValue(&hadc1);
          HAL_ADC_Stop(&hadc1);
  }
  /* USER CODE END 3 */
}
 
This code works perfectly for NUCLEO-L433RC-P and NUCLEO-L476RG, but it doesn't work on NUCLEO-F103RB. I would like to know why is that. On F103RB board first ADC channel shows correct readings and second channel just shows the same value as first channel.
This topic has been closed for replies.
TDK
TDKBest answer
Aug 18, 2023 1:17 PM UTC

> sConfig.Rank = ADC_REGULAR_RANK_2;

If you're only converting a single channel, this should be ADC_REGULAR_RANK_1.

> sConfig.SamplingTime = ADC_SAMPLETIME_1CYCLE_5

Consider increasing this. Also, you should initialize it in your ADC_Select_CH2 function, otherwise it will have an undefined value.

"If you feel a post has answered your question, please click ""Accept as Solution""."

1 reply

TDK
TDKBest answer
Aug 18, 2023 1:17 PM UTC

> sConfig.Rank = ADC_REGULAR_RANK_2;

If you're only converting a single channel, this should be ADC_REGULAR_RANK_1.

> sConfig.SamplingTime = ADC_SAMPLETIME_1CYCLE_5

Consider increasing this. Also, you should initialize it in your ADC_Select_CH2 function, otherwise it will have an undefined value.

"If you feel a post has answered your question, please click ""Accept as Solution""."