Skip to main content
Associate
October 13, 2023
Solved

STM32 and Platformio

I have been developing a program for the Nucleo-32 (STM32L412KBU6) board in Visual Studio Code's Platformio, and I have run into an interesting problem. I am able to build my project with no errors and upload it successfully. However, whenever the code is uploaded to the board, the program does not run. The only way that I can get it to run is by using the debugger to walk step by step through the code. Does anyone know of a solution to this strange issue? (I can drop my code here in a zipped file if I need to).

 

Thanks, in advance, for the help.

This topic has been closed for replies.
TDK
TDKBest answer
October 16, 2023

Different compilers will produce different code. Just because one of them "worked" doesn't imply the code is bug free.

Suggest remaining objective and debugging the issue at hand directly.

"If you feel a post has answered your question, please click ""Accept as Solution""."

3 replies

TDK
October 13, 2023

Probably a bug in the code. Attach a debugger without resetting to see where it's at.

 

"If you feel a post has answered your question, please click ""Accept as Solution""."
caden013Author
Associate
October 16, 2023

I know there isn't an issue with the code because I copied and pasted the same code into Keil uVision5 and uploaded it to the board, and it worked with no problems. It has to be an issue with Visual Studio Code and Platformio.

TDK
TDKBest answer
October 16, 2023

Different compilers will produce different code. Just because one of them "worked" doesn't imply the code is bug free.

Suggest remaining objective and debugging the issue at hand directly.

"If you feel a post has answered your question, please click ""Accept as Solution""."